Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Re-annotating hierarchical sheets
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 90 subscribers
  • Views 4798 views
  • Users 0 members are here
  • hierarchical design
  • re-annotate
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Re-annotating hierarchical sheets

awardautomation
awardautomation over 9 years ago

Ok so if you use Hierarchical Sheets to add multiple instances of the same schematic block, you will obviously get duplicate designators on your pcb layout.

CS solves this by adding a suffix to the component designators, consisting of an underscore and the designator you used for the sheet symbol.

The only problem is the designator names get a bit long, and take up real estate on your board.

I was trying to reduce designators lengths by re-annotating the PCB, then using -> Update the Schematic from PCB.

ECO window correctly matches the names and reports that it has worked but in fact it only changes the main sheet.

If you look in the tabs along the bottom of the sub sheet you will see the designators are unchanged.

Has anyone found a workaround for this?

  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 9 years ago +2 verified
    The naming style used for designators can be changed using Home > Project > Options > Multi-channel, see below for settings for a more compact representation.
  • awardautomation
    awardautomation over 9 years ago in reply to e14softwareuk +1
    This is great! Thanks Peter The best way I found to use this was to start numbering in the sub-sheet from R1, D1 etc, and to use A,B,C as designators of my sheets. This way the composite name ends up as…
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to bugrobotics +1 suggested
    Not sure you can reproduce the example board behaviour without manually assignment. It is possible to mess with the assignments to get just numeric designators like below. This might not be a great example…
Parents
  • e14softwareuk
    0 e14softwareuk over 9 years ago

    The naming style used for designators can be changed using Home > Project > Options > Multi-channel, see below for settings for a more compact representation.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • bugrobotics
    0 bugrobotics over 7 years ago in reply to e14softwareuk

    Hi Peter,
    How would one go about getting the behavior shown in the example project (PCB_PCIe_4-Port...) where the separate channel's components get annotated with a simple number?  The example project doesn't seem to follow it's own settings (Multi-Channel project options: $Component_$ChannelName). 

     

    EDIT:

    Maybe a clue...I see where the annotation has been set manually (pic below).  Any ideas?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • bugrobotics
    0 bugrobotics over 7 years ago in reply to e14softwareuk

    Hi Peter,
    How would one go about getting the behavior shown in the example project (PCB_PCIe_4-Port...) where the separate channel's components get annotated with a simple number?  The example project doesn't seem to follow it's own settings (Multi-Channel project options: $Component_$ChannelName). 

     

    EDIT:

    Maybe a clue...I see where the annotation has been set manually (pic below).  Any ideas?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to bugrobotics

    Not sure you can reproduce the example board behaviour without manually assignment. It is possible to mess with the assignments to get just numeric designators like below. This might not be a great example given there seems great potential for name clashes.