Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Adjust Solder Mask Expansion from PCBLIB Inspector
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 2174 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Adjust Solder Mask Expansion from PCBLIB Inspector

tomridl
tomridl over 9 years ago

Hi,

 

I am trying to adjust the solder mask expansion value from the PCBLIB Inspector, but there is only a checkbox to for "Solder Mask Override", and then no where to enter the override value. This means that to adjust the solder mask expansion, you have to manually change it for every pin instead of for all pins at once. Please could you add the option to adjust this for all the selected pins in the inspector, as per full Altium. Bit of a mission changing 100 pins manually! Does anyone know of another way to do this without using the inspector?

 

Thanks

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 9 years ago

    Hi Thomas, you can set the solder mask expansion in the PCB editor using Home > Design Rules; Mask > Solder Mask Expansion rule set. The override option is typically used when you need to set a few special pins with a different value to the rules you have defined.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tomridl
    0 tomridl over 9 years ago in reply to e14softwareuk

    Hi Peter, thanks for the reply.

     

    This will then change the solder mask expansion for all components (which I don't want to do). If I have only one fine pitch component that needs to be different to the default, then it seems I have to do each pin manually. It seems strange that there is a checkbox in the PCBLIB Inspector to override the default, but no place to enter in the override value!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tomridl
    0 tomridl over 9 years ago in reply to e14softwareuk

    Hi Peter, thanks for the reply.

     

    This will then change the solder mask expansion for all components (which I don't want to do). If I have only one fine pitch component that needs to be different to the default, then it seems I have to do each pin manually. It seems strange that there is a checkbox in the PCBLIB Inspector to override the default, but no place to enter in the override value!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 9 years ago in reply to tomridl

    If there is one specific component then you can add a design rules to set a different expansion and apply the rule to either a named component (ref des) or footprint.If you are trying to set up in the library editor you can set the properties for a pad to specify a mask expansion value using the radio button and then entering a value (see image).