Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to eliminate warnings about and display of power pins on components with multiple parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 91 subscribers
  • Views 5355 views
  • Users 0 members are here
  • multi-part
  • power pin
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to eliminate warnings about and display of power pins on components with multiple parts

lamabrew
lamabrew over 8 years ago

I'm pretty sure I've overlooked something obvious.

 

As an example, place an op-amp from Vault. After placing the A part CS seems to switch to placing the B part for you. However it shows power pins too:

image

Same thing if you also place each part from Vault. If you compile the schematic it throws Duplicate Pin warnings about the power pins. If I open up the properties for the B part and edit the pins and hide the power pins the warnings go away, but the symbol still shows pins:

 

image

 

My questions:

  • Is there a way to have CS automatically not include power pins after the first sub-part is placed?
  • Is there a way to remove/hide the extra lines like shown on the B part above?

 

Thanks

  • Cancel
Parents
  • jimku
    0 jimku over 8 years ago

    I have created schematic symbols with multiple parts with power pins on only one of the parts and have never had a problem with the power pins showing up on the other parts. Something that I think that I am doing differently from what you describe is that I place the power pins on the last gate of the multi-part part. I just briefly tried it again to see what would happen or if something changed since the last time I created a multi-part symbol but it worked fine as expected. When I created the schematic symbol I created part A without power pins. I then created part B and then added the power pins. Compile and save. I then place part A first in the schematic and then part B. I do the same with multi-part logic where I create all the parts without the power pins and add the power pins to the last symbol of the multi-part device. Power pins then show up only once per multi-part device which is the last part of the package.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to jimku

    Jim, this is exactly how I used to create multi-part symbols. Define all the gates then have a power part and perhaps other common / misc pins. However the parts in question are vault parts which cannot easily be modified so I think either stick with how the vault works and wire up all the power pins to eliminate the compiler warnings or define your own parts in whatever style you wish.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to jimku

    Jim, this is exactly how I used to create multi-part symbols. Define all the gates then have a power part and perhaps other common / misc pins. However the parts in question are vault parts which cannot easily be modified so I think either stick with how the vault works and wire up all the power pins to eliminate the compiler warnings or define your own parts in whatever style you wish.