Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Moving tab to new window is not working?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 93 subscribers
  • Views 3272 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Moving tab to new window is not working?

jaxxs
jaxxs over 8 years ago

Hello

 

First post here.

 

So I was once able to open a tab into a new window, have that window on another monitor and I could simple drag tabs from the main window to the new window.

I can no longer do this and I have to open each tab into it's own window. The drag icon suggests that it should be able but on release...nothing?

I'm not sure if it's due to a windows 10 Update as the current CS version was working but is no longer working?

 

Any help is much appreciated

 

Cheers,

Mark

  • Cancel

Top Replies

  • bugrobotics
    bugrobotics over 8 years ago in reply to e14softwareuk +1
    e14softwareuk wrote: Just to update everyone that it appears possible the latest Windows 10 version 1709 update may cause issues with CircuitStudio multi-monitor support but is still under investigation…
  • bugrobotics
    bugrobotics over 8 years ago in reply to e14softwareuk +1
    Ill preface my response by saying I know you have nothing to do with all of this, you're just doing your job and I mean no disrespect. Pointing to another developer who has the same issues is like saying…
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    Hi Mark and welcome to the CircuitStudio forums. I'm using Windows 7 and the multi-monitor support is working fine for me, there is no need to already have a second window opened, I can just drag a document tab onto another monitor (into any empty space on the desktop) and it will launch CircuitStudio on that monitor and host the dragged document. Dragging a tab to a second already opened CircuitStudio works fine too, have you tried dropping onto different areas of the CS window just in case it makes any difference?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mars01
    0 mars01 over 8 years ago in reply to e14softwareuk

    Hi,

     

    I have windows 10 x64 with latest updates. The reported behavior is happening to me also on two different computers.

     

    If  I drag the CS tab from the primary monitor into a second monitor space it will not create a new instance of the CIrcuitStudio to host the new tab.

    If I right click on the tab and then click on "Open in a new window" option then the tab is opened into a new instance of CS, as desired.

     

    Now, if I try to redock the tab from the second instance of CS to the first instance of CS, it will not comply and it will stay in the second instance of CS. As a result in the primary instance of CS (the original one) in the place were the tab should be redocked (the last position on the tab bar) a black bar will appear, like in the attachment.

     

    More than this, the tabs on the original instance of CS can't be reordered. As an example, I can't drag a tab from first position to the last and so on. It doesn't matter if I have only one instance of CS or two.

     

    Peter, you can reproduce this issue by trying to use the software on Windows 10 x64 with all updates. Trying to drag the tab in any part of the monitor space doesn't change the reported behavior.

     

    LE: As a second thought, I looked and there is no mention in the System Requirements of CircuitStudio that Windows 10 is supported.

    There is only:

    "Below are the recommended and minimum system requirements to install and run CircuitStudio.

    Recommended System Requirements

    • Windows 7 or Windows 8 (32-bit or 64-bit)

    "

    Should we assume that Windows 10 is not supported?

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to mars01

    Thanks for the extra info, I have passed on to Altium to ask their technical people to check if latest Win 10 has broken something. If anyone else on the forums has started experiencing the same after it was working then please post so that we can see if this is a general problem or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to mars01

    Windows 10 is supported, the last 1.4.1 release included several fixes to improve compatibility with Win 10 to keep up with the changes that Microsoft keep making to the platform. This could be just another case of Microsoft making breaking changes to some of their APIs.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to mars01

    Just to update everyone that it appears possible the latest Windows 10 version 1709 update may cause issues with CircuitStudio multi-monitor support but is still under investigation.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • bugrobotics
    0 bugrobotics over 8 years ago in reply to e14softwareuk

    e14softwareuk  wrote:

     

    Just to update everyone that it appears possible the latest Windows 10 version 1709 update may cause issues with CircuitStudio multi-monitor support but is still under investigation.

     

    I have close to 40 programs installed on my Windows 10 machine and none of them have issues like CS.  CS caused my first BSOD in 7 years!  The reason for this comment is that it appears as though blame continues to be placed on Windows 10 when the problem is most likely the way that CS is built.  Other programs (Solidworks/Fusion 360/ Photoshop/Draftsight/Simplify3D/HSMWorks/GWizard/etc) work just fine through these updates.

     

    If I am way off base I'd welcome a technical explanation.  This sort of comment can't make potential buyers or current maintenance subscribers comfortable and certainly pushes me away from renewing maintenance.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to bugrobotics

    You must be quite lucky, just take a look at at this article where a well known CAD vendor recommends not to install the latest Win 10.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • bugrobotics
    0 bugrobotics over 8 years ago in reply to e14softwareuk

    Ill preface my response by saying I know you have nothing to do with all of this, you're just doing your job and I mean no disrespect.

     

    Pointing to another developer who has the same issues is like saying "See, they have an inferior platform too" (I use a few different Autodesk products regularly, on Win/Mac, without issue).  Something is causing all the issues with CS. There have been many documented on this forum, big and small.  The blue screen is probably the most severe with all of the minor issues like the vault windows, people not being able to access licenses, etc being less important. The software seems to be an afterthought and quickly thrown together.

     

    All software has issues, especially in the beginning. The issue I have is the response, or lack of response, by Altium.  The whole setup for the support is strange.  The lack of a roadmap for the updates/planned changes is bizarre.  I may stand on my own on this but something about the situation doesn't feel right.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • tarribred61
    0 tarribred61 over 8 years ago in reply to e14softwareuk

    I have Win10 build 1709 and it is working for me.  I use a laptop with 2 extra external monitors for a total of 3.  I tested opening up some of the tabs on another window and then putting moving tabs between the windows.

     

    I'm not saying it doesn't work but it is at least working for some of us.  That may make it difficult to debug for them.

     

    When I drag a tab I get a little black bar that show where it will go if I drop it. (screen shot below).  When I release it will drop as expected.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jaxxs
    0 jaxxs over 8 years ago in reply to tarribred61

    I'm using Windows10 (Home) build 1709, so I guess this further complicates things?

     

    I get the same feedback as you have posted, just no tab is shown when it's dropped but the solid black line remains?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
>