Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum screen resolution and pop-up windows not fitting on screen
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 89 subscribers
  • Views 2517 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

screen resolution and pop-up windows not fitting on screen

motorman2018
motorman2018 over 8 years ago

I am on the trial for CircuitStudio and was working on making a new component. In the schematic editor I got my square for the part but when I want to add a pin and press TAB to get to the pin properties window, it pops up but too far up on the screen and the top line is invisible. I cannot drag the window down because the top is off the screen. Running W10 and screen resolution of 3200x1800.

 

Anybody seen this before and what to do to fix this?

Attachments:
image
  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 8 years ago +1 suggested
    Although running a very high resolution screen Windows is scaling the application making it effectively run at low resolution. Best idea would be to adjust the scaling settings in Windows. For moving the…
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    Although running a very high resolution screen Windows is scaling the application making it effectively run at low resolution. Best idea would be to adjust the scaling settings in Windows. For moving the dialog as shown in the image try using the standard Windows keyboard commands: ALT+SPACE followed by M and then the cursor (arrow) keys to move the dialog window.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • motorman2018
    0 motorman2018 over 8 years ago in reply to e14softwareuk

    Thanks Peter, this is a good solution for the problem.