Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum PCB component edit window too large to fit screen
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 4 replies
  • Subscribers 89 subscribers
  • Views 1717 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

PCB component edit window too large to fit screen

opeongo73
opeongo73 over 8 years ago

When editing a component in the pcb layout format, the window that opens is too large for my screen. At the top, it starts at the line X-Location and at the bottom it stops at Vault Name. The window is frozen and cannot be moved. However, I can change values within the part that is visible and hit return and it saves it. I am using Windows 7 Pro. with a screen resolution of 1600X900. I think this was working before so I must have done something to cause this.

 

Any suggestions.

Thanks.

  • Cancel

Top Replies

  • e14softwareuk
    e14softwareuk over 8 years ago +1
    Hi Jim. I've just checked and the component property dialog will fit a 900px tall screen, the screenshot shows how it should look on 1440x900 monitor. This is not a resizable dialog so I would guess your…
Parents
  • opeongo73
    0 opeongo73 over 8 years ago

    Thanks for the reply Peter. I have checked my resolution and it is set to 1600X900 however, I don't see where I can set the scaling factor. I have checked one of the supplied demos and when I check the component, it still truncates the top and bottom of the component property dialog so it must be my system that is doing this.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to opeongo73

    There should be an option in the Windows control panel, check under Display or similar. The graphics card driver might also have its own software that can affect scaling.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • opeongo73
    0 opeongo73 over 8 years ago in reply to e14softwareuk

    I found it. Here are the steps.

    1) Control Panel-Click on "Ease of access" then select "Optimize visual display"

    2) Click on "Change the size of text and icons"

    3) Click on Smaller 100% (default) and apply. (Mine was set to 125%)

     

    This will correct the "component property dialog" window size so that it appears properly.

    Thanks Peter.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • opeongo73
    0 opeongo73 over 8 years ago in reply to e14softwareuk

    I found it. Here are the steps.

    1) Control Panel-Click on "Ease of access" then select "Optimize visual display"

    2) Click on "Change the size of text and icons"

    3) Click on Smaller 100% (default) and apply. (Mine was set to 125%)

     

    This will correct the "component property dialog" window size so that it appears properly.

    Thanks Peter.