Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to set the columns for a pick and place file?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 90 subscribers
  • Views 2536 views
  • Users 0 members are here
  • part id
  • pick and place
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to set the columns for a pick and place file?

lamabrew
lamabrew over 8 years ago

Sorry if this has an obvious answer somewhere but so far I haven't found it.  This document: Pick and Place Data Format  shows the default which assumes a part number in the comment field (which IMHO is kind of a bad default as the comment field seems to be the only way to get a text field between schematic and layout for labeling things like connectors, etc. so can't be used for part info).

 

However my part numbers are in a custom "Part ID" field this is used to map between schematic components and the real world.  I can't find  a template file or dialog to set this.

 

How do you set the configuration of the generator to use the correct data field?

 

Altium Designer help shows a dialog to select the fields, I can't find that in CS.

  • Cancel
  • voltsandjolts
    0 voltsandjolts over 8 years ago

    Use the BOM generator to generate a PnP file as described here:

     

    http://valhalla.altium.com/Learning-Guides/OG0104%20Pick%20and%20Place%20Output%20Options.pdf

     

    Note:

    At the bottom of the BOM setup dialog, tick "Include parameters from PCB".

    That will add component position parameters to the list of available fields (centre X, centre Y etc) so you can build a custom formatted PnP.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • lamabrew
    0 lamabrew over 8 years ago in reply to voltsandjolts

    Yeah I saw that option discussed in a couple of places and is going to be my fallback.

     

    Though a tad annoying that a program for creating PCBs can't easily create the files needed to assemble them. There's a lot to like about CS but this one really does have me confused in a what were they thinking kind of way. But you seem to be confirming what I see elsewhere that the custom BOM generator is the best solution.

     

    Thanks for the advice.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • lamabrew
    0 lamabrew over 8 years ago in reply to lamabrew

    Self followup for anyone else looking for more info. I think these are the most helpful directions on how to use the BOM generator to create a pick and place file.

    https://resources.altium.com/pcb-design-blog/creating-a-custom-pick-and-place-file

     

    I couldn't find a way to attach the .XLT file but these are the columns I used:

     

    Column=DesignatorColumn=FootprintColumn=Center-X(mm)Column=Center-Y(mm)Column=Ref-X(mm)Column=Ref-Y(mm)Column=Pad-X(mm)Column=Pad-Y(mm)Column=LayerColumn=RotationColumn=CSPID

     

    Replace the last one with whatever your part number field is. (don't' forget the ' on the entries so Excel doesn't think they're equations).