Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Route to a pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 91 subscribers
  • Views 2660 views
  • Users 0 members are here
  • routing
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Route to a pad

baudot
baudot over 8 years ago

I'm trying to make an ultra-simple break-out board: Every pin on a surface-mount chip goes to a pad on a PCB, so I can solder male headers into the pads for easy prototyping on a solderless breadboard.

 

The problem is, when I try to route from the chip's pins to the pads, the route dodges the pad! (See attached image.)

The mouse acquires a symbol, crossed wires, when I try to make the connection. (For reasons unknown, my screen-grab tool doesn't grab it.)

 

My suspicion is that since the pad was added in the PCB editor, and the schematic is literally just the chip, with no connections, the PCB editor thinks it should indeed be a floating pin, connected to nothing.

 

How do I get around this? How do I route from a chip to a pad that I've added in the PCB editor window?

Attachments:
image
  • Cancel
Parents
  • mars01
    0 mars01 over 8 years ago

    I recommend to do what the previous answers said but if you really, really want to do what you proposed to do then go to: File -> System Preferences -> PCB Editor -> Routing Conflict Resolutions -> Current Mode and in the drop-down menu select Ignore obstacles. This will allow you to cross with the track over a pad not in the same net. You'll see the connections marked with a white circle and shortcircuit symbol but it will work if the only thing you want is to do a toner transfer PCB image

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to mars01

    To add to this suggestion of using Ignore Obstacles, once you have completed your routing use Tools | Netlist > Configure Physical Nets. This brings up a dialog that lets you turn the copper into actual nets. Gets rid of the short circuit indicators.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to mars01

    To add to this suggestion of using Ignore Obstacles, once you have completed your routing use Tools | Netlist > Configure Physical Nets. This brings up a dialog that lets you turn the copper into actual nets. Gets rid of the short circuit indicators.