Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Route to a pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 91 subscribers
  • Views 2658 views
  • Users 0 members are here
  • routing
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Route to a pad

baudot
baudot over 8 years ago

I'm trying to make an ultra-simple break-out board: Every pin on a surface-mount chip goes to a pad on a PCB, so I can solder male headers into the pads for easy prototyping on a solderless breadboard.

 

The problem is, when I try to route from the chip's pins to the pads, the route dodges the pad! (See attached image.)

The mouse acquires a symbol, crossed wires, when I try to make the connection. (For reasons unknown, my screen-grab tool doesn't grab it.)

 

My suspicion is that since the pad was added in the PCB editor, and the schematic is literally just the chip, with no connections, the PCB editor thinks it should indeed be a floating pin, connected to nothing.

 

How do I get around this? How do I route from a chip to a pad that I've added in the PCB editor window?

Attachments:
image
  • Cancel
Parents
  • baudot
    0 baudot over 8 years ago

    Workaround in this case: Remove the pads from the PCB, add headers as a component to the schematic, and wire them together.

     

    Still, what's the point of being able to add pads on the fly in the PCB editor if you can't connect to them? Surely you can, and I'm missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 8 years ago in reply to baudot

    As you don't have a full schematic that means you probably don't have any nets defined either. You can't connect to the pad because it is not assigned to the net of the track you are editing. You can double click each pad and assign a net for it. You can get the net name from the tracks you create or create all nets in Tools> Netlist > Edit. Probably easier just to create your pad layout as a component and do a proper schematic. 10 mins.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • baudot
    0 baudot over 8 years ago in reply to voltsandjolts

    Thanks. As a new user, it took me a bit to figure out one or two less obvious things about this. (Mostly that I had to add a 0-length unlabeled pin to the pad to make it a connection point.)

     

    This answer got me where I needed to be.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • baudot
    0 baudot over 8 years ago in reply to voltsandjolts

    Thanks. As a new user, it took me a bit to figure out one or two less obvious things about this. (Mostly that I had to add a 0-length unlabeled pin to the pad to make it a connection point.)

     

    This answer got me where I needed to be.