Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum setting via's net bug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 16 replies
  • Subscribers 92 subscribers
  • Views 3110 views
  • Users 0 members are here
  • frontpage
  • bugs
  • bug
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

setting via's net bug

Sparkylabs
Sparkylabs over 8 years ago

So i am trying to add some GND vias onto what is already a polygon pour of a different net. So I start my via placement and press tab before placing so that I can pick the net, choose my net, place the via and hey presto my explicit instructions are ignored..... Any chance this ever gets fixed?

  • Cancel

Top Replies

  • Sparkylabs
    Sparkylabs over 8 years ago in reply to bugrobotics +1
    Normally copy and paste produces a copy (clue is in the name) is CS you get something different. It's like word copying text but changing the font. If i didn't want that net why would i do the copy? I…
Parents
  • Sparkylabs
    0 Sparkylabs over 8 years ago

    I think my problem was because I was placing vias over an area that could have been to different nets, which is why i took the trouble to specify it, pity altium could not take the trouble to code their software to do as told..... copy and paste is just that, if things had of worked first time as they should have I would not have been trying to copy and paste and even that does not work as it should.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • Sparkylabs
    0 Sparkylabs over 8 years ago

    I think my problem was because I was placing vias over an area that could have been to different nets, which is why i took the trouble to specify it, pity altium could not take the trouble to code their software to do as told..... copy and paste is just that, if things had of worked first time as they should have I would not have been trying to copy and paste and even that does not work as it should.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • jaza_tom
    0 jaza_tom over 8 years ago in reply to Sparkylabs

    I think you are correct.

     

    e14softwareuk  here is a video showing the described behaviour.

     

    In my example, I am trying to add GND vias, and I am doing so in an area where there are two internal layers with polygon pours underneath: 5V and GND

     

    The vias' Net property keep getting overidden to 5V even though I explicitly set the parameter to GND during placement.

     

    The only viable workaround I have found is to do one of the following:

     

    - Move the offending polygon pour off your board temporarily, taking note of it's X/Y position so you can easily move it back later

    - Change the way you are adding vias.  Instead of dropping via using the Via placement tool, use the route tool, route a track from the desired pad, and then switch layer to GND layer, which automatically drops a via tied to GND net the next time you click

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    0 voltsandjolts over 8 years ago in reply to jaza_tom

    Or another way, as I suggested above, place the vias outside the board then drag them to where you need them.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to jaza_tom

    You are correct in that placing a via onto a polygon (poured or unpoured) does reassign the net. To add to the workarounds you can change the polygon layer to a spare mechanical layer so that it does not interfere with via placement and then change layer back afterwards. This way you do not need to remember the coordinates for the polygon because it never moved.