Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Recomendations on panelization software for user array and multiproject?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 92 subscribers
  • Views 2945 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Recomendations on panelization software for user array and multiproject?

lamabrew
lamabrew over 7 years ago

After experimenting with the PCB fab house doing the panelizing and the back and forth that entailed, and not getting quite consistent results, I want to take a stab at doing the creation of a user array. I'm using that term to not confuse with the panelizing the fabricator does to put N user boards on a typical raw material blank.

 

For now I'm just interested in making either 2 up (1x2) or 4 up (2x2) array of the same board design - 10mm rails with tooling/fids, routed edges with tabs type thing.

 

Down the road I may want to make a multi-project (i.e. 2 different designs) user array as some of the boards always end up in pairs. In that case though I also need to provide the assembly house with a merged pick and place file with all the offsets correct. I can offset the ref-des' easily enough.

 

I want some tool to generate the panels and DRC the whole thing, etc., hopefully one tool that handles both the N copy user array as well as the N project user array.

 

There are a number of tools out there but they seemed to be more aimed at fabricators and/or have a lot of high end features that aren't needed for 2 or 4 layer boards with >= 6/6 rules. In other words I don't want to spend more on the tool than I spent on CircuitStudio.

 

Hoping someone here might have figured this out and could share what they do.

 

Thanks for any suggestions.

 

Brewster

  • Cancel

Top Replies

  • lamabrew
    lamabrew over 7 years ago in reply to mars01 +1
    Hi Marius, Thank you for the information. It certainly looks promising. I poked around for an AD created embedded array file (some posts said some were on EEVBlog) but didn't turn any up. I know someone…
  • mars01
    mars01 over 7 years ago in reply to bugrobotics +1
    In this case, in the link below you'll find both: - Altium Designer PcbDoc file binary 5.0 (that can be imported by CS) with Embedded board arrays (I've added 3 of them but you can copy them as much as…
  • mars01
    mars01 over 6 years ago in reply to nickverlooy +1 suggested
    Hi Nick, Here is a MEGA link for the file that I've posted above but it is no longer available on that location. https://mega.nz/#!Iop1QAwI!jYsFDiK2PGWofVL3pVxiM3JYQuvzYAhElIuqrtwvfU4 Best, Marius
Parents
  • nickverlooy
    0 nickverlooy over 6 years ago

    Can you please send me a template like this?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mars01
    0 mars01 over 6 years ago in reply to nickverlooy

    Hi Nick,

    Here is a MEGA link for the file that I've posted above but it is no longer available on that location.

    https://mega.nz/#!Iop1QAwI!jYsFDiK2PGWofVL3pVxiM3JYQuvzYAhElIuqrtwvfU4

     

    Best,

    Marius

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • mars01
    0 mars01 over 6 years ago in reply to nickverlooy

    Hi Nick,

    Here is a MEGA link for the file that I've posted above but it is no longer available on that location.

    https://mega.nz/#!Iop1QAwI!jYsFDiK2PGWofVL3pVxiM3JYQuvzYAhElIuqrtwvfU4

     

    Best,

    Marius

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • lamabrew
    0 lamabrew over 6 years ago in reply to mars01

    Marius: I'm still using that template you posted back when I started this thread.  Thanks for keeping the file available (I've kind of given up hope that Altium will update CS to allow PCB arrays).

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mars01
    0 mars01 over 6 years ago in reply to lamabrew

    Hi Brewster,

    For the past two years I took over the development for the open-source software FlatCAM (www.flatcam.org). My focus was in adding everything that is needed to make PCB prototyping at home (or work) easy but I've added there a tool (sort of plugin) named Panelization Tool. You can panelize Gerber/Excellon files very easy and then save the resulting object(s) as Gerber(s)/Excellon(s). Sometime in the near feature I will add a tool that will add tear drops too.My efforts result is what is called now FlatCAM beta, currently at version 8.98.

     

    As for Circuit Studio development ... it's a long time now since I understood the situation. It was like a river slowly drying to a trickle. Until there is nothing anymore. At least I have an Altium Designer license available from work image. They've just renewed subscription so I am waiting to see AD v 20.

    • Cancel
    • Vote Up 0 Vote Down