Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to assign multiple PCB footprint pads to a single pin on a schematic library component
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 2 replies
  • Subscribers 90 subscribers
  • Views 4869 views
  • Users 0 members are here
  • pin
  • netlist
  • circuit studio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to assign multiple PCB footprint pads to a single pin on a schematic library component

jaza_tom
jaza_tom over 7 years ago

I'm trying to figure out how to assign multiple pads to a single pin on a schematic library component.

 

So far, my strategy has been to simply add extra hidden pins to the schematic symbol for the component that are placed directly on top of their matching partner pin.  Then when you go to wire up the schematic, placing a wire to that pin should connect both the hidden and visible pin to that net, right?

 

At least that's how my logic went.

 

Apparently, this is not the case, as can be seen in the below video (note that you will probably have to choose a high resolution from the video settings dialogue popup in order to properly view video):

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

So, if my method is not the way to accomplish this, then what is the preferred method?

  • Cancel
Parents
  • adamwebber
    0 adamwebber over 7 years ago

    You could change the footprint in the footprint editor.  When numbering the pads, just make pad number 1 and then make another pad number 1.  Now you have two pads that are number 1.  When you link it to your schematic library component, all pads that are labeled with number 1 will be attached to pin 1.  Simple.  This is also helpful when making other types off footprints for packages where there is a backplane and also a pin connection like T0-220 packages where the middle pin is also connected to the backplane.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • adamwebber
    0 adamwebber over 7 years ago

    You could change the footprint in the footprint editor.  When numbering the pads, just make pad number 1 and then make another pad number 1.  Now you have two pads that are number 1.  When you link it to your schematic library component, all pads that are labeled with number 1 will be attached to pin 1.  Simple.  This is also helpful when making other types off footprints for packages where there is a backplane and also a pin connection like T0-220 packages where the middle pin is also connected to the backplane.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • jaza_tom
    0 jaza_tom over 7 years ago in reply to adamwebber

    Thanks!