Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum odb++ output issues with circuitstudio
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 94 subscribers
  • Views 5255 views
  • Users 0 members are here
  • circuitstudio
  • odb++
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

odb++ output issues with circuitstudio

doov123
doov123 over 8 years ago

I'm having issues with CircuitStudio and odb++ output generation.  For some reason my supplier and I can both not view the odb++ outputs from CS (gerbers/pick and place files work fine).  Whenever I try to open the odb++ files (I'm using the "standard" viewer: https://www.odb-sa.com/resources/odb-viewer/ ) I get the following error "get-112113-illegal import file was detected" (screen shot attached).  I saw this note: ODB++ output formatting issues in CS , but I'm not sure it's related since a quick scan of the directory structure doesn't appear to have uppercase letters.  Has anyone successfully outputted odb++ from CS and been able to view them?  

Attachments:
image
  • Cancel

Top Replies

  • hlovett
    hlovett over 7 years ago +1
    I've tracked this problem down to Circuit Studio not exporting a font file, for some reason. Fix is to (manually) place a font file in the fonts folder in the ODB++ structure. Then re zip or tar-ball the…
Parents
  • hlovett
    0 hlovett over 7 years ago

    I've tracked this problem down to Circuit Studio not exporting a font file, for some reason.

     

    Fix is to (manually) place a font file in the fonts folder in the ODB++ structure. Then re zip or tar-ball the files up and it all works!

     

    I've attached the standard font file to help.

     

    EDIT: you may need to remove the .txt extension for it to work in other ODB++ viewers

    Attachments:
    standard.txt.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to hlovett

    Very interesting. Were there any other changes you needed to make? Were you using the free ODB++Viewer 10.1? Just adding in the font file doesn't seem to be enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • hlovett
    0 hlovett over 7 years ago in reply to e14softwareuk

    No - I just added that and put it into a zip archive

    Have you removed the .txt extension? (so it is extensionless?) and it looks like the forum has zipped the file too - I assume you have extracted it as well?

     

    I'm using a slightly newer version of the free viewer - ODB++ Viewer 11. Maybe that's worth a try?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tueftler@work
    0 tueftler@work over 7 years ago in reply to e14softwareuk

    Same here.

    I've delete the file extension and copy the file "standard" into the font folder.

    After compressing and opening in "ODB++ viewer 10.2" a error message comes up with text "ge_valor-12504-Illegal entity name".

     

    I can open the file with any editor and can read the plain text, so it is decompressed correctly.

     

    That's too bad image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • hlovett
    0 hlovett over 7 years ago in reply to tueftler@work

    Are you tar balling or zipping?

     

    I've just zipped it, without the fonts file and it opens okay in Viewer 11.

    Re-tarballing to tar.gz using 7zip seems to work okay also...

    Might have had a red-herring here with the fonts file.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • hlovett
    0 hlovett over 7 years ago in reply to tueftler@work

    Are you tar balling or zipping?

     

    I've just zipped it, without the fonts file and it opens okay in Viewer 11.

    Re-tarballing to tar.gz using 7zip seems to work okay also...

    Might have had a red-herring here with the fonts file.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to hlovett

    Mixed success using version 11 in that some designs have worked and others fail.