Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Parts not transferring from schematic to board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 90 subscribers
  • Views 3100 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Parts not transferring from schematic to board

ahbushnell@hotmail.com
ahbushnell@hotmail.com over 7 years ago

I have a diode component in my schematic.  I first put in four of the diodes and then transfered them to the PCB with no problem.  I then latter tried to transfer more of the same diode and they don't transfer?  I have had this problem before. 

 

Any suggestions?

 

Andy

  • Cancel

Top Replies

  • adamwebber
    adamwebber over 7 years ago in reply to ahbushnell@hotmail.com +1 verified
    I vaguely remember something like this happening to me while using Altium many years ago. Each time I would update the PCB from the Schematics, the same parts would get erased and I would need to lay them…
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to ahbushnell@hotmail.com +1 suggested
    I would recommend running the Components Links command in the PCB editor. This checks the integrity of links between the schematic and PCB components and allows you to fix-up any discrepancies.
Parents
  • ahbushnell@hotmail.com
    0 ahbushnell@hotmail.com over 7 years ago

    I think there are bugs here. 

     

    But I managed to make it work.

     

    It's related to when you copy parts in a schematic.  Sometimes it works sometimes it doesn't.  I found if I place each part from the library instead of copying in the schematic it works better.

     

    Another problem I observed.  When parts are imported from the schematic to the PCBA sometimes the nets get confused.  For instance one capacitor will have the wrong net attached and the other capacitor will have no nets.  If I deleted those two components from the PCBA and then re-import  it seems to fix it. 

     

    Hopefully 1.6 will come out soon and fix these problems. 

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to ahbushnell@hotmail.com

    I would recommend running the Components Links command in the PCB editor. This checks the integrity of links between the schematic and PCB components and allows you to fix-up any discrepancies.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • ahbushnell@hotmail.com
    0 ahbushnell@hotmail.com over 7 years ago in reply to e14softwareuk

    That's very helpful.

     

    It's a manual fix for the bug.  Hopefully they will fix the bug.

     

    This will help if there is a part in the PCBA that is not linked to a component in the schematic. Which I have had trouble with  But I was having the problem of parts not appearing in the PCBA. 

     

    Thanks

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • ahbushnell@hotmail.com
    0 ahbushnell@hotmail.com over 7 years ago in reply to e14softwareuk

    That's very helpful.

     

    It's a manual fix for the bug.  Hopefully they will fix the bug.

     

    This will help if there is a part in the PCBA that is not linked to a component in the schematic. Which I have had trouble with  But I was having the problem of parts not appearing in the PCBA. 

     

    Thanks

     

    Andy