Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How to create Design Rule for Poly and Trace to Board Edge
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 763 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How to create Design Rule for Poly and Trace to Board Edge

sclifford
sclifford over 7 years ago

I am trying to create Design Rule for Poly to Board Edge.  I do not see any were to select a board edge to create this design rule.

 

Scott

  • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago

    Typically you would place a copy of the board outline on the global Keepout Layer to which rules can apply.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • sclifford
    0 sclifford over 7 years ago in reply to e14softwareuk

    Peter,

    I am used to Altium and there is a layer dedicated for the board outline.  In CS I do not see a layer dedicated just to the board, in CS is this layer called "Outline"?

    My question comes from when you say make a copy of the board outline to create a keep-out area.  I do not see this in my layout,  were i can even see the board outline noted as a color.  I notice it appears when I edit the board outline but this is the only time.  Note I am trying to create an automatic ability to re leave copper pours from my board edges so they can be sealed by solider mask.  Sorry i am used to doing this in Altium but a bit confused as to how to get this accomplished in CS.

     

    Thanks

    Scott Clifford

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to sclifford

    Board outlines can be a confusion subject as there are so many of them!! There is the '3D' board outline defined using Home | Board Shape which gives the colouring to the workspace areas and the 3D view; the Outline layer which is typically used to hold a copy of the board outline for Gerber file generation and Keepout Layer which is typically used as a global keepout and is a copy of the board outline. It is possible to copy the 3D outline to a normal layer (Home | Board Shape > Create Primitives from Board Shape) and create the 3D outline from a collection of shapes (Home | Board Shape > Define From Selected Objects).