Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Pad to pad rules exception for the same component - HOW?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 91 subscribers
  • Views 5881 views
  • Users 0 members are here
  • pad
  • pad clearance
  • design rules
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Pad to pad rules exception for the same component - HOW?

olemi
olemi over 7 years ago

Did someone figure out how to configure exception from the pad-to-pad clearance rule for a given components or just the same components in general?

 

image

  • Cancel
Parents
  • frog
    0 frog over 7 years ago

    To the best of my knowledge you can't do this (and I'm not an authority on the subject) but it raises the question of why would you want such an exception.  If that spacing is acceptable on one place then why not in any other place?  To the best of my knowledge you could create a design rule that allows a smaller spacing for those two nets, or to allow a smaller spacing between SM pads specifically (which is perhaps the closest thing to what you really want).

    image

    Were it me I'd change the offending pads (or all of them for that matter) to rounded rectangle as per IPC recommendations.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • olemi
    0 olemi over 7 years ago in reply to frog

    It's standard practice to limit spacing 0.2mm to be at the edge of manufacturer's capabilities for the whole design and avoid crossed PCB on the panel, but have ICs with smaller spacing on the same design. The soft really need "pad-to-pad for the same component" rule. Limitation by nets will not work well. Additionally, it's a pain to configure 64 rules for a 64-pins IC. Indeed, spacing between SMD pads is the closest, but then DRC will not check pads of different components. I though about a workaround where I would need to draw a courtyard around each component at the distance half of what I need between pads of different components with following courtyard-to-courtyard DRC Rule, but I didn't find any suitable rule. Which rules stands for component-to-components? Courtyard is responsible for controlling spacing between components?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to olemi

    There is a separate rule category for component clearance under Placement > Component Clearance.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • olemi
    0 olemi over 7 years ago in reply to e14softwareuk

    They don't work for that purpose. They are based on 3D models. This is, btw, wrong solution - pads can go far from components shape. Averaging is not applicable here, all components are different. For components clearance the only correct way is to check outlines or courtyards clearance. So, I guess no workaround here expect setting pad-to-pad high globally.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 7 years ago in reply to olemi

    The component clearance can be based on 3D models but you can draw an outline (e.g. courtyard top) that can be used to help with clearance - the horizontal clearance rule.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • olemi
    0 olemi over 7 years ago in reply to e14softwareuk

    The horizontal clearance for placement rule? It doesn't work. I can put courtyard on courtyard.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • olemi
    0 olemi over 7 years ago in reply to e14softwareuk

    The horizontal clearance for placement rule? It doesn't work. I can put courtyard on courtyard.