Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Can't Select and Modify Wires but Components are selectable
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 90 subscribers
  • Views 2096 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Can't Select and Modify Wires but Components are selectable

rpruitt76
rpruitt76 over 7 years ago

Have an interesting problem. Well more frustrating...On one of my schematics, I can't select or modify my wires. I can place additional wires but one they are placed, I can't move them or select them. The problem is more bizarre in that if I open the same schematic file from another Laptop running another variant of Circuit Studio, that package has full access to my wires and can select and modify them.

 

Suspect Laptop running Circuit Studio under Windows 10 is running version 1.5.2 (Build 30)

 

Laptop running Circuit Studio where wires are selectable is also running Windows 10 running version 1.2.0 (Build 37)

 

Any advice would be greatly appreciated.

 

Thanks

  • Cancel
Parents
  • dexter23
    0 dexter23 over 7 years ago

    As e14softwareuk said,

     

    I see that on your suspect laptop you are running v1.5 and an older version on the other pc.

    In V1.5 they introduced these selection filters (so your other PC does not have the filter option), in many cases (during PCB editing) i find them a blessing, but in the beginning i had the same frustration like you when i forgot to check the filter setting.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • dexter23
    0 dexter23 over 7 years ago

    As e14softwareuk said,

     

    I see that on your suspect laptop you are running v1.5 and an older version on the other pc.

    In V1.5 they introduced these selection filters (so your other PC does not have the filter option), in many cases (during PCB editing) i find them a blessing, but in the beginning i had the same frustration like you when i forgot to check the filter setting.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • clem57
    0 clem57 over 7 years ago in reply to dexter23

    Good catch  . So have the correct type of cursor like other programs like adobe PDF viewer. e14softwareuk & dexter23