Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Interactive routing bug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 2 replies
  • Subscribers 89 subscribers
  • Views 1195 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Interactive routing bug

mo.abdol
mo.abdol over 7 years ago

 

I have come across a situation with unexpected (and certainly undesirable) behavior. The issue  has been observed by other users, but no solution has been proposed, as explained below:

The project is a 4-Layer design (Top, L1, L2, Bottom) where L1 and L2 are designated as "Internal planes". I am trying to route signals from a BGA device on the Bottom Later to the Internal Plane L2. To achieve this, I have placed u-Vias directly at the center of the BGA pads. The intent is that these u-Vias take the signal from the Bottom Layer to L2, and then I route them on the L2 Layer. For the layers, I have specified two sets of Drill-pairs; the default (Through Via) which goes from the Top Layer to the Bottom Layer, and for the u-Vias going from L2 Layer to the Bottom Layer.

The strange behaviors that I see are listed below:

1) When I select the L2 Layer, as soon as I start interactive routing, the software jumps to the Bottom Layer and adds whatever trace I draw to the Bottom Layer
2) If I try to change the properties of the trace that is added in Step 1) above so that it is placed on the L2 Layer, the net selection does not remain. For example, when I edit the properties and assign the GND net to the selected trace, I click OK to save the editing. Then, when I check the properties, the net is shown as "no net", as if I never edited the property

Can anyone provide some suggestions or workarounds?

Thanks in advance,

Mo

 

  • Cancel
  • voltsandjolts
    0 voltsandjolts over 7 years ago

    Internal plane layers are only for power and ground nets, you can't place traces on them. You should be using a polygon pour instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    0 tarribred61 over 7 years ago

    V&J is right.  Maybe change the internal plane layers into signal layers and then you should be able to route on them.  Also, in case you didn't do it or for others that don't know, for a 4-layer board with blind vias on outer layers you need to make the outer layer pairs the core style and have the pre-preg in the center.