Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Polygon not connecting to Pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 9 replies
  • Subscribers 91 subscribers
  • Views 6709 views
  • Users 0 members are here
  • relief
  • polygon pour
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Polygon not connecting to Pad

dbemmann
dbemmann over 6 years ago

Strangely the pads of my component are not connecting to polygons of the same net. Why?

 

The component (J2 on the screenshot) is a self-designed solder-jumper defined as a net tie. On this PCB I want to use it to connect two ground planes (polygons with nets GND and AGND). As you can see, CircuitStudio doesn't connect the pads to the polygons.

 

Both polygons are set to "pour over all same net objects". I have two design rules for "polygon connect style":

Priority 1: first object = via, second object = all, connect style = direct connect

Priority 2: first object = all, second object = all, connect style = relief

 

You can both of them working on the other pads, but strangely not on the solder-jumper. On the other hand, these fine unrouted lines show that it should be connected. What am I doing wrong? Just for completeness, the component is built with 4 pads (two rounded ones overlapped by two rectangular ones). In any case there is enough room for relief lines.

image

  • Cancel
Parents
  • laska
    0 laska over 6 years ago

    Are you sure that all 4 pads are connected to proper ground? I suggest to reduce number of pads to 2 and check, if the problem still exist.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • laska
    0 laska over 6 years ago

    Are you sure that all 4 pads are connected to proper ground? I suggest to reduce number of pads to 2 and check, if the problem still exist.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • dbemmann
    0 dbemmann over 6 years ago in reply to laska

    All 4 pads have the correct "Name" in the component editor (the left pads both have "1" and the right pads a "2") which translate to GND, GND, AGND, AGND in the PCB (as can be seen when zooming further in), and that's all correct. I tried what you suggested anyways (only one pad on each side). The problem still exists.