Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Polygon not connecting to Pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 9 replies
  • Subscribers 91 subscribers
  • Views 6709 views
  • Users 0 members are here
  • relief
  • polygon pour
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Polygon not connecting to Pad

dbemmann
dbemmann over 6 years ago

Strangely the pads of my component are not connecting to polygons of the same net. Why?

 

The component (J2 on the screenshot) is a self-designed solder-jumper defined as a net tie. On this PCB I want to use it to connect two ground planes (polygons with nets GND and AGND). As you can see, CircuitStudio doesn't connect the pads to the polygons.

 

Both polygons are set to "pour over all same net objects". I have two design rules for "polygon connect style":

Priority 1: first object = via, second object = all, connect style = direct connect

Priority 2: first object = all, second object = all, connect style = relief

 

You can both of them working on the other pads, but strangely not on the solder-jumper. On the other hand, these fine unrouted lines show that it should be connected. What am I doing wrong? Just for completeness, the component is built with 4 pads (two rounded ones overlapped by two rectangular ones). In any case there is enough room for relief lines.

image

  • Cancel
Parents
  • voltsandjolts
    0 voltsandjolts over 6 years ago

    I haven't had problems with net ties connecting to poly pours, so it can work.

    The "solder bridge" component type should be "Net Tie". It should be a component, not just two pads of different nets with a track drawn between them.

    If you placed the track between GND and AGND, the clearance rules are likely keeping the poly pours away.

    You could also try: Tools > Netlist > Updates Free Primitives From Component Pads

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • dbemmann
    0 dbemmann over 6 years ago in reply to voltsandjolts

    The whole thing (the 4 pads and the little track between them) are a component and I defined it as a Net Tie. There is no extra track connected to the pads in the PCB (other than the bridge in the middle which is part of the component). Isn't that the correct way? I tried "Update Free Primitives From Component Pads" and also re-poured. It didn't have any effect.

     

    What clearance rule do I need? I have just the default one in place with the numbers altered. I found that if in the matrix of that clearance rule, I change the value for "Poly - SMD Pad", it doesn't affect those particular pads, and not the other GND pad in the picture either, probably because the rule also contains "Different nets only". But anyways, looking at that other GND pad, we can see how big the clearance is and how wide the relief is, and there would be space for that in my net tie, so I don't understand why it's not connecting.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • dbemmann
    0 dbemmann over 6 years ago in reply to voltsandjolts

    The whole thing (the 4 pads and the little track between them) are a component and I defined it as a Net Tie. There is no extra track connected to the pads in the PCB (other than the bridge in the middle which is part of the component). Isn't that the correct way? I tried "Update Free Primitives From Component Pads" and also re-poured. It didn't have any effect.

     

    What clearance rule do I need? I have just the default one in place with the numbers altered. I found that if in the matrix of that clearance rule, I change the value for "Poly - SMD Pad", it doesn't affect those particular pads, and not the other GND pad in the picture either, probably because the rule also contains "Different nets only". But anyways, looking at that other GND pad, we can see how big the clearance is and how wide the relief is, and there would be space for that in my net tie, so I don't understand why it's not connecting.