Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Unwanted/confusing net selection by "select connected copper"
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 2 replies
  • Subscribers 88 subscribers
  • Views 1207 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Unwanted/confusing net selection by "select connected copper"

jonasss
jonasss over 6 years ago

Hi Everyone,

 

I'm having a hard time figuring out what's going on with the "select connected copper" tool.

 

In the picture below I use this tool and it selects all the tracks from connection a to b, just like expected.

 

image

 

But when I then edit the track - purpose is for length matching - and I use the same tool "select connected copper" it selects all GND tracks as seen in the following picture.

 

image

 

There is no obvious connection from the track that I want to connect (SDX2) to that GND. Am I missing something?

 

When I use "select physical connection" it then selects the tracks correct from a to b, like expected. BUT the select connected copper also selects other nets, which is a real scary thing!

 

 

Any help much appreciated!

 

Best Regards

 

Jonas

 

 

Edit:

 

Has anyone else observed this behaviour?

It seems like the function "select connected copper" is useless. This happens with pretty all other nets, too. For example, the actual selected net (selected with "select connected copper") selects multiple nets, which clearly have nothing to do with each other as seen in the picture:

image

 

Nachricht geändert durch Jonas Burghardt

  • Cancel
Parents
  • tarribred61
    0 tarribred61 over 6 years ago

    Hi,

     

    I'm not sure.  It works for me when I have used this but I have not used it much.  Testing just now on a board and it seems to work as expected even if I move things a bit.

     

    Could you have some issues with the netlist?  Is there polygon that needs repour?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tarribred61
    0 tarribred61 over 6 years ago

    Hi,

     

    I'm not sure.  It works for me when I have used this but I have not used it much.  Testing just now on a board and it seems to work as expected even if I move things a bit.

     

    Could you have some issues with the netlist?  Is there polygon that needs repour?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • tarribred61
    0 tarribred61 over 6 years ago in reply to tarribred61

    One of the ways I check lengths is to use the PCB panel and look at the routed and un-routed lengths. You can use the up and down arrows to cycle through the nets to see how they are routed also. If you try this make sure your selection filter is set to all objects.

     

    image

    If you hold the shift key and pick the nets in the list it add the nets (more than one) to highlight.