Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Circuit Studio :: Mixed mode Simulation included?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 1312 views
  • Users 0 members are here
  • simulation
  • mixed
  • circuitstudio
  • mode
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Circuit Studio :: Mixed mode Simulation included?

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I've a question about Circuit Studio:

 

You write that this software includes "Mixed mode simulation capabilities are included right from inside the tool" ; which is not written on CST website.

I tried free Trial and didn't see this feature neither ; even if component have linked sim parameters, there is no Simulation panel.

+Source libraries sim are not included.

 

So is it really a feature of this software or not?

and how to proceed?

 

Tks.

  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    finny, The Mixed Mode Simulation is officially being tested in Beta right now for the v1.1 release. This will be available in mid-May. Along with the simulation, we have added:

     

    - Additional Importers - Updated to include Protel, PCAD, and support for Altium .PCBDOC (AD10 and older)

    - .STEP export ability

    - DXF import ability

     

    Thanks for your participation here and your evaluation of CircuitStudio!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I am currently evaluating the software and I can't for the life of me find any command that will allow me to start a simulation. I have built a very simple schematic using a couple of parts that have simulation models, but don't see any way to run the simulation. Is this part of the software package yet? The version I downloaded is 1.1.0 (build 44421). I keep reading that simulation was supposed to be added in May of this year.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I am currently evaluating the software and I can't for the life of me find any command that will allow me to start a simulation. I have built a very simple schematic using a couple of parts that have simulation models, but don't see any way to run the simulation. Is this part of the software package yet? The version I downloaded is 1.1.0 (build 44421). I keep reading that simulation was supposed to be added in May of this year.