Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum IMPORT DXF FILE TO CIRCUIT STUDIO V1.1
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 92 subscribers
  • Views 5126 views
  • Users 0 members are here
  • dxf
  • circuitstudio
  • import
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

IMPORT DXF FILE TO CIRCUIT STUDIO V1.1

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I want to import a DXF file to circuit studio v1.1. I tried it but it doesn't work. In the new version 1.1 is supposed it is possible to import DXF files. So I did the following:

I selected File>import and I browse to find the required file. Once I click in the required file, one small window appears saying "done", but the board's shape doesn't appear in my new blank PCB. Am I doing anything wrong?

Looking forward to hearing from you

Best regards

Javier

  • Cancel

Top Replies

  • e14softwareteam
    e14softwareteam over 9 years ago in reply to erix +1
    Apologies for the delay Eric. This was just resolved over email. There are normally two main reasons why the DXF file doesn’t import correctly and for you the second was the solution: 1- The import may…
Parents
  • erix
    0 erix over 9 years ago

    I just received an email from support that solved the problem. I will paste it here so that all who search the internet looking for a fix will find it:

     

    "You may need to uninstall/reinstall the installation of TeighaX, the installer is located at C:\Program Files (x86)\Altium\CS\System\Installation\TeighaX_Setup_3.9.0.msi. TeighaX is a 3rd party utility used during import of dxf/dwg."

     

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • erix
    0 erix over 9 years ago

    I just received an email from support that solved the problem. I will paste it here so that all who search the internet looking for a fix will find it:

     

    "You may need to uninstall/reinstall the installation of TeighaX, the installer is located at C:\Program Files (x86)\Altium\CS\System\Installation\TeighaX_Setup_3.9.0.msi. TeighaX is a 3rd party utility used during import of dxf/dwg."

     

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareteam
    0 e14softwareteam over 9 years ago in reply to erix

    Apologies for the delay Eric.  This was just resolved over email.  There are normally two main reasons why the DXF file doesn’t import correctly and for you the second was the solution:

     

    1- The import may have completed, but at a VERY small scale. Try Zooming in to see if the image then shows up. If it does you may have to readjust your scale settings. 2- You may need to uninstall/reinstall the installation of TeighaX, the installer is located at C:\Program Files (x86)\Altium\CS\System\Installation\TeighaX_Setup_3.9.0.msi. TeighaX is a 3rd party utility used during import of dxf/dwg.  Setting the correct scale and installing/repairing TeighaX should get things working

     

    Best,

    e14SoftwareTeam

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • harvie256
    0 harvie256 over 9 years ago in reply to erix

    Thanks for making this information public.  My install also had not installed TeighaX.

     

    e14softwareteam In future it's of great help to your users to make this information public at the earliest opportunity.  If this answer was posted here with the original posters question, then many of us would have saved time.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareteam
    0 e14softwareteam over 9 years ago in reply to harvie256

    Will do harvie256, we appreciate the feedback!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • dahlback
    0 dahlback over 9 years ago in reply to e14softwareteam

    Hi,

     

    The second option solved my problem with the import.

    Thanks!

     

    Best regards,

    Robin

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • vadim007
    0 vadim007 over 9 years ago in reply to e14softwareteam

    Thank you, guys! You save my day.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • fuubar67
    0 fuubar67 over 9 years ago in reply to e14softwareteam

    That helped allot image Happy ster having to import step files for a year. The reinstall worked.