Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Is there a way to import a vault component into a local library ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 94 subscribers
  • Views 7243 views
  • Users 0 members are here
  • circuitstudio
  • altium_vault
  • import
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Is there a way to import a vault component into a local library ?

e14 Contributor
e14 Contributor over 11 years ago

I don't like the idea of being dependant of external, cloud based libraries.

Internet is not always available, or sometimes it's very slow.

Altium vault is free at the moment, but this might change.

Symbols in the vault are not always drawn as we would like (pins arrangement, size, etc...)

So, is there a way to get a part and models, store them in our own local libs, and if needed edit them ?

 

Jacques in Brussels

  • Cancel

Top Replies

  • awardautomation
    awardautomation over 9 years ago in reply to oliver@drive.ai +2 suggested
    Agreed Oliver... the UI is not self-explanatory as we have come to expect from modern packages. It requires a lot of googling around to find the secret method of doing very simple things. This symptomatic…
  • mflux_gamble
    mflux_gamble over 9 years ago in reply to djam +1
    This isn't correct as far as I can tell. In Altium there is an ability to right click on a PCBlib or SCHlib component in the Vault, select operations >> clone. you cannot do this in CS. its very frustrating…
  • bugrobotics
    bugrobotics over 9 years ago in reply to mflux_gamble +1
    Agreed, this is basic functionality that needs to be added. Component creation is a mess currently. Creation/copying existing components needs to be simple.
Parents
  • djam
    0 djam over 10 years ago

    Hi Jacques,

     

    Once a symbol or footprint is part of a Schematic or PCB, all you need is stored in those files.

     

    To add it to your own library, you can copy it from the editor (PCB or Schematic), and paste it

    into the list in the Library panel, (the Library panel associated with the library file when open).

    You can even do it for multiple symbols/footprints at a time.

     

    Regards,

    Darren

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mflux_gamble
    0 mflux_gamble over 9 years ago in reply to djam

    This isn't correct as far as I can tell.

     

    In Altium there is an ability to right click on a PCBlib or SCHlib component in the Vault, select operations >> clone.  you cannot do this in CS.  its very frustrating.  It would be great to have access to especially the footprints - so at the very least we could copy generic package type footprints and edit them.

    I have a need to make a 3x3mm tssop 8 pin foot print.  I found one chip in the vault that uses this footprint.  guess what, no way to copy it.  wtf.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • mflux_gamble
    0 mflux_gamble over 9 years ago in reply to djam

    This isn't correct as far as I can tell.

     

    In Altium there is an ability to right click on a PCBlib or SCHlib component in the Vault, select operations >> clone.  you cannot do this in CS.  its very frustrating.  It would be great to have access to especially the footprints - so at the very least we could copy generic package type footprints and edit them.

    I have a need to make a 3x3mm tssop 8 pin foot print.  I found one chip in the vault that uses this footprint.  guess what, no way to copy it.  wtf.