Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Wires won't connect?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 2 replies
  • Subscribers 89 subscribers
  • Views 3308 views
  • Users 0 members are here
  • wires
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Wires won't connect?

jgauthier
jgauthier over 4 years ago

I did a bunch of work in a schematic and ran into multiple issues when adapting to the PCB.

One of those issues is that some of my components don't have wires attached to them.   When I inspect them in the schematic, I can *see* wires, but they don't appear to be connected.

For example, take a look at this:

image

So, I press "W" and connect the wire.

image

Then I move the wire...

image

Nope, not connected.  I mean, Why is this so hard?  The other side of the component has two grounds and they are fine. But both pins on this side won't connect.

There's no feed back to tell me something is wrong, there's no visual indication it did not connect.

  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 4 years ago +4
    It looks like the part (D3?) has been created with the pins the wrong way around. The four dots at the end of the pin mark the connection point or 'hot spot' of the pin, see Section 6 of this: https:/…
Parents
  • e14 Contributor
    e14 Contributor over 4 years ago

    It looks like the part (D3?) has been created with the pins the wrong way around. The four dots at the end of the pin mark the connection point or 'hot spot' of the pin, see Section 6 of this: https://my.altium.com/altium-designer/getting-started/local-library-and-symbol-creation. Normally pins butt against the edge of the part graphic, with the hot spots on the outside (see the reg below) and wires attach to the hot spots. The wire is trying to get to the connection point but can't make it 'into' the body of the component.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 4 years ago

    It looks like the part (D3?) has been created with the pins the wrong way around. The four dots at the end of the pin mark the connection point or 'hot spot' of the pin, see Section 6 of this: https://my.altium.com/altium-designer/getting-started/local-library-and-symbol-creation. Normally pins butt against the edge of the part graphic, with the hot spots on the outside (see the reg below) and wires attach to the hot spots. The wire is trying to get to the connection point but can't make it 'into' the body of the component.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Children
  • jgauthier
    jgauthier over 4 years ago in reply to e14 Contributor

    Yes, figured it out late last night!  Thank you for the confirmation!