Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum ANSI B printing and generating PDFs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 11 replies
  • Subscribers 89 subscribers
  • Views 4023 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ANSI B printing and generating PDFs

eng101
eng101 over 4 years ago

I'm trying to print schematic sheets using the Project > Generate Outputs workflow and the page sizes are all scaled incorrectly such that the schematic only takes up a portion of the page.

There are a bunch of topics on this in the forum but no definitive answers other than it might be something to do with the printer drivers. I've uninstalled every printer, deleted them from the registry, reinstalled Circuit Studio, (doing a clean uninstall that deleted all of my saved preferences and settings), deleted the OutJob files for the projects and yet it keeps doing it on every single project. Does anyone have a definitive solution for this or a printer driver that I can use that is known to work?

  • Cancel

Top Replies

  • eng101
    eng101 over 4 years ago in reply to shabaz +1
    I appreciate the response, several other people are using it here without issue but I haven't been able to replicate their configuration or figure out what's different on mine so I don't believe it's an…
  • tarribred61
    tarribred61 over 4 years ago in reply to eng101 +1
    Maybe you can post a screen shot of what your print config settings are?
  • NHEE2
    NHEE2 over 4 years ago +1
    Ok, had time to play so I took a look at this. I can easily cause a B size sheet to print on 4 sheets of a pdf files by NOT checking "fit document on page" in page setup in project outputs with schematic…
Parents
  • bills_alsentis
    bills_alsentis over 4 years ago

    So here's my process for creating B size Schematic sheets - if I follow this process, it seems to work every time......

    • Schematic Print/PDF Export (B Size Sheet):
      • CS > Outputs Tab > Print
        • Select Microsoft Print to PDF
        • Cancel - Do Not print yet!
      • CS > Outputs Tab > Page Setup:
        • Select Tabloid, Landscape, Fit, Color
      • CS > Outputs Tab > Print > Microsoft Print to PDF > Properties
        • Select Landscape, Advanced > Paper Size > Tabloid
        • Print to the file
      • Print the generated file to the printer using Adobe Acrobat Reader
        • Select Ledger under Page Setup in the lower left corner of the dialog

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • eng101
    eng101 over 4 years ago in reply to bills_alsentis

    I appreciate the response, but I have no issues with printing single schematic sheets using Outputs > Print however this feature is only a single schematic page at a time and more importantly it does not contain the embedded component information (part number, vendor etc.). To get all schematic sheets in a single file along with the embedded component information you have to use the Projects > Generate Outputs > Schematic Prints dialog, and unfortunately this is the one that doesn't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • eng101
    eng101 over 4 years ago in reply to bills_alsentis

    I appreciate the response, but I have no issues with printing single schematic sheets using Outputs > Print however this feature is only a single schematic page at a time and more importantly it does not contain the embedded component information (part number, vendor etc.). To get all schematic sheets in a single file along with the embedded component information you have to use the Projects > Generate Outputs > Schematic Prints dialog, and unfortunately this is the one that doesn't work.