Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Countersink holes in PCB
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 10 replies
  • Subscribers 89 subscribers
  • Views 3654 views
  • Users 0 members are here
  • circuitstudio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Countersink holes in PCB

jgauthier
jgauthier over 4 years ago

Is it possible to create a countersink hole with CircuitStudio?

  • Cancel

Top Replies

  • NHEE2
    NHEE2 over 4 years ago in reply to Andrew J +1
    Probably depends on the FAB house. You may move from drilling, routing over to a manual operation department. Particles of PCB material and copper may contaminate otherwise pristine surfaces, causing scratches…
  • NHEE2
    NHEE2 over 4 years ago in reply to dougw +1
    Treat your countersunk hole as any other part with a single hole. The diameter should be the thru hole diameter you need for your screws. The hole should be unplated and no pads on any layer. Now this…
  • jgauthier
    jgauthier over 4 years ago in reply to NHEE2 +1
    HAHA. Thanks for your answer. I liked the last part. The answer is some vendor sent us a CAD drawing of their board and it had countersink holes (I never saw it - I only have the actual board). Our Mechanical…
Parents
  • Andrew J
    Andrew J over 4 years ago

    Interesting question.  Is it actually possible to get a PCB manufacturer to create countersunk holes in a PCB?  

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • dougw
    dougw over 4 years ago in reply to Andrew J

    It is definitely possible and some shops will do it.

    It does take more specification than a normal hole because Gerbers are just 2 dimensional, but modern PCBs are really 3 dimensional products. The removed material doesn't create any more issues than any other milling operation on the PCB, such as slots or even regular drilled holes..

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • NHEE2
    NHEE2 over 4 years ago in reply to dougw

    Treat your countersunk hole as any other part with a single hole.  The diameter should be the thru hole diameter you need for your screws.  The hole should be unplated and no pads on any layer.  Now this will give you the placement and FAB accuracy you need.  Specify your countersink details only on the fab drawing using the same method you would for solid metal or sheet metal part.  This include countersink angle and the depth of the countersink operation.

    As an aside, why do you want or need countersunk holes?  If you're hoping for more accurate board alignment, you may see that OR, the first screw that's tightened down will lock an X/Y coordinate.  The other holes will be trying to pull the board in their direction.  For a frightening 50 years of product development, I've never used other than pan/binding head screws and helical lock washer if needed, or snap in plastic fasteners for lower cost products.  Or in some cases, mounting holes may fit over injection molded "pins" in your design, eliminating hardware.

    But perhaps you have a need for flushness on one side of the assembly.

    But also, it's none of my business :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to NHEE2

    If the question was directed it me, I don't need countersunk holes I just thought it was an interesting original question as I hadn't come across any specific means to do so in Kicad - the only PCB app I've used.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • NHEE2
    NHEE2 over 4 years ago in reply to Andrew J

    Sorry, my mistake and I didn't see a way to redirect it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • NHEE2
    NHEE2 over 4 years ago in reply to Andrew J

    Sorry, my mistake and I didn't see a way to redirect it.