Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How do you remove a duplicate image that is below datum line. Doesn't show up in Circuit Studio (doesn't show below datum) but shows up in Gerbers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 3 replies
  • Subscribers 88 subscribers
  • Views 945 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How do you remove a duplicate image that is below datum line. Doesn't show up in Circuit Studio (doesn't show below datum) but shows up in Gerbers?

sshaferdlm
sshaferdlm over 4 years ago

imageimage

  • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago

    Maybe try:

    Select everything (maybe ctrl-a works, I don't speak Circuit Studio)

    Un-select everything visible

    Now move the still selected parts that are out of view up and left until they show up above the datum line. It is a little bit of a guessing game. Or instead of moving try delete the still selected things that are out of view.

    Good luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • sshaferdlm
    sshaferdlm over 4 years ago

    I have tried that and not able to select. Circuit Studio appears not to allow anything to be see below datum.

    I have also tried to just edit the Gerbers however Circuit Studio does not come with Gerber editor.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 4 years ago in reply to sshaferdlm

    I'm guessing you already tried this but... if you know what layer the graphics are on, then use the Home > Select all on layer to select everything. 

    image

    Alternative is to use the search window and type in select and it should pull up the command

    image

    You can then delete the entire layer.  Of course you don't want to delete the stuff that is in view and above the datum so select that first and use the PCB inspector to change it to a different layer such as an empty mechanical layer.

    If the stuff won't delete then it is possible it is locked so it would not get selected.  In that case you may need to change the settings to disable protect locked objects. That is under the File > System Preferences > PCB Editor > General settings window.

    As a final resort, you could select all the PCB stuff on all the layers and copy it into a new PCB file.  Then rename (later delete) the old one and rename the new one back to your project.  You probably have to regenerate your drill table and layer stackups.

    If you still can't delete it, you can probably just leave it.  The PCB house may call you but it should not impact the layers related to the PCB.  Or call them first and let them know about it ahead of time.

    There is an open source Gerber viewer from GEDA called gerbv that might help delete it.  I use it to view Gerbers but I have not edited with it.