Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum polygon region short circuit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 23 replies
  • Subscribers 88 subscribers
  • Views 7108 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

polygon region short circuit

acw210ee
acw210ee over 3 years ago

So i have polygons overlapping each other connected to nets, it seemed to draw them fine with J1 in the pcb however i get the DRC i get a short errors:

Clearance Constraint (Gap=6mil) (All),(All)
Polygon Region (93 hole(s)) Bottom Layer Pad J1-1(2129.921mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-1(2129.921mil,-459.134mil) Multi-Layer
Polygon Region (93 hole(s)) Bottom Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (48 hole(s)) Top Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer


Back to top

Short-Circuit Constraint (Allowed=No) (All),(All)
Polygon Region (93 hole(s)) Bottom Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (88 hole(s)) Signal Layer 2 Pad J1-3(1870.079mil,-459.134mil) Multi-Layer
Polygon Region (48 hole(s)) Top Layer Pad J1-3(1870.079mil,-459.134mil) Multi-Layer

When i remove J1 the problem goes away, however i am not sure what is causing it. As the issue with the polygon pours does not occur with the ot

her components. Should i just ignore the issue?

image

  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    The answer is no. A DRC error should never be ignored unless the reason for it is known and either corrected or acknowledged. In your case, since the reason is not known, it is not reasonable to ignore it.

    I don't use Circuit Studio (KiCad is better supported even through community support), so I'm not 100% sure of the reason.

    image

    What are all the small red circles? Are they the way Circuit Studio indicates an error, or are they very small top layer circular pads? If they are pads, they are exceedingly small. 

    Circuit Studio may use the concept of polygon 'priority' or 'rank' (other CAD packages do). It may be worth altering such a priority in case that is somehow causing a short.

    One more thing worth doing sometimes is to proceed with generating Gerber files, and then inspecting them in a Gerber viewer. Sometimes the problem area can be more easily identified from there.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Hi,

    The answer is no. A DRC error should never be ignored unless the reason for it is known and either corrected or acknowledged. In your case, since the reason is not known, it is not reasonable to ignore it.

    I don't use Circuit Studio (KiCad is better supported even through community support), so I'm not 100% sure of the reason.

    image

    What are all the small red circles? Are they the way Circuit Studio indicates an error, or are they very small top layer circular pads? If they are pads, they are exceedingly small. 

    Circuit Studio may use the concept of polygon 'priority' or 'rank' (other CAD packages do). It may be worth altering such a priority in case that is somehow causing a short.

    One more thing worth doing sometimes is to proceed with generating Gerber files, and then inspecting them in a Gerber viewer. Sometimes the problem area can be more easily identified from there.