Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Jump Component and View Configurations Hotkeys
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 9 replies
  • Subscribers 93 subscribers
  • Views 3121 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Jump Component and View Configurations Hotkeys

spe672
spe672 over 9 years ago

In Altium Designer PCB view, you can press "J" "C" and that opens a text box where you can type in a ref des and your cursor will "jump" to point at the component on your PCB.  Can I do this in CS with some other keystrokes?

 

ALSO, pressing L in Altium will bring up the "View Configurations" window.  In CS, I have to double click the active layer button in the lower left.  Is there any way to set up hotkeys?  I don't find anything in the preferences area.

 

Thanks!

Andy

  • Cancel
Parents
  • solidcore
    solidcore over 9 years ago

    Hello Andy,

     

    Unfortunately, Circuit Studio has fairly limited hotkeys and menu shortcut keys, as compared to Altium Designer due to the ribbon-style interface vs menu-style interface. However, I do agree that they should at least allow customization of shortcut keys due to this limitation.

     

    In terms of Jump to Component, the only workaround that I found is using the command search on the top right corner to execute the command and open up the prompt window.

     

    image

    Not sure what PeterC meant above because I was not able to hit l to bring up the View configurations window in CS Version 1.3 either. My method is by single-clicking the colored box right beside the "LS" key.

    image

    Please let me know how this goes for you, thank you.

     

    Regards,

    Eu Jin

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to solidcore

    I confess that I am now using Solidworks PCB which as far as I'm aware is essentially a clone of Circuit Studio.

    Apart from having more limitations (like no access to the Vault) I had not found any other differences.

     

    The lower case L definitely works in this.

     

    Apologies if I raised hopes....

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • spe672
    spe672 over 9 years ago in reply to e14 Contributor

    NP, I expected L to work as well.  It's been that way in Altium Designer and Protel before it since the 90's.  Why not incorporate that into CS?  I don't get it. 

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • rspcb
    rspcb over 9 years ago in reply to spe672

    I access the View Configurations dialogue approximately once every 10 minutes (sometimes more). Are we the only ones that use this so often? The omission of a hotkey seems silly, I also cant wait to try SHFT+L thanks for the tip

     

    It's a bummer the config files are not directly compatible with Altium, I don't see the benefit of having to re-create them if you move from CS up to AD. It's very handy to flip between placement views and routing views with different layers active to minimize the visual noise.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • rspcb
    rspcb over 9 years ago in reply to spe672

    I access the View Configurations dialogue approximately once every 10 minutes (sometimes more). Are we the only ones that use this so often? The omission of a hotkey seems silly, I also cant wait to try SHFT+L thanks for the tip

     

    It's a bummer the config files are not directly compatible with Altium, I don't see the benefit of having to re-create them if you move from CS up to AD. It's very handy to flip between placement views and routing views with different layers active to minimize the visual noise.