Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Polygons - automatic repour on error
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 13 replies
  • Subscribers 93 subscribers
  • Views 4386 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Polygons - automatic repour on error

GilchristT
GilchristT over 9 years ago

Folks

 

Am I missing something or is the "Automatic repour on polygon error" setting missing from the PCB Editor -> General settings screen?

 

If you make a change that requires a polygon repour the dialog gives you the option to change the setting but it's not there in version 1.4 unless I'm being particularly slow today?

  • Cancel

Top Replies

  • GilchristT
    GilchristT over 9 years ago in reply to e14softwareteam +1
    Sorry but I think you've missed my point. I've no problems repouring polygons, I just use the standard repour now and that resolves the issue. To give an example, say I've created a board design, placed…
Parents
  • vadim007
    vadim007 over 7 years ago

    This annoying window has been driving me crazy for years already. image Please, add an option to disable it in future releases.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to vadim007

    Polygon re-pours are so slow on all but the most trivial of boards, trying to work with auto re-pours would drive me insane(r).

    Pouring polys is the very last thing I do on a board.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • mars01
    mars01 over 7 years ago in reply to voltsandjolts

    Hi @voltsandjolts,

     

    If CS performance is bothering you, then you could run the DXP.exe (CS executable) with high priority. From I what I saw, CS is run mainly on a single thread/processor and running the executable as high priority will help.

     

    From another forum I learned that you could automate this by using a small open-source utility named 'Bat to Exe Converter' which can be downloaded from here: Bat To Exe Converter | F2KO Software

    From the same forum (it's another user work, I only copy/paste here) the BAT file should look like this:

     

    @echo off
    IF [%1] == [] (
    Start "Altium Circuit Studio" /high "C:\Program Files (x86)\Altium\CS\DXP.orig.EXE"
    REM echo "There is no input file"
    ) ELSE (
    Start "Altium Circuit Studio" /high "C:\Program Files (x86)\Altium\CS\DXP.orig.EXE" %1
    REM echo "Input file is %1"
    )
    REM pause

     

    assuming that your CS installation folder is the default one.

     

    Using this BAT as a source you will create a new DXP.exe file which is more or less an "shortcut" to the real DXP.exe file which now needs to be renamed to DXP.orig.exe

     

    You also need to rename the following files from:

    dxp.exe.config

    DXP.exe.manifest

     

    to:

    dxp.orig.exe.config

    DXP.orig.exe.manifest

     

    You can still run the CS as you used to but this time you do it from the renamed file: DXP.orig.exe

    If you want to run CS as a high priority process you do it from the new "shortcut" DXP.exe

     

    If you trust running an executable from an outside source I post here a link with the small executable that I just created through the same process just described (and also tested it). I also found and used  in this executable the CS icon.

    If you use the file in the following link, unzip it and remember also to rename the original files as mentioned above.

    https://cp.sync.com/dl/79aeb2b00/chvma4pg-3bqfmduj-tqdf98p9-h8v38qri

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to mars01

    Interesting idea - have you seen any difference in performance by using a higher process priority. I would have thought that it would not make much difference unless you are seriously multitasking on your computer. It would be great to get a comparison if it boost performance.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to mars01

    Thanks for the info on process priority, however, for pouring polys it made no difference for me.

    I'm running a HP Z-book i7-7820HQ 16GB.

    The board I'm working on (approx 100x150mm) takes 8 seconds to pour two large polys, 4 secs to repour.

    Making the dxp process high priority didn't speed this up unfortunately.

     

    Who knows, maybe the CS code is pour_poly() then sleep(4000). That would not surprise me.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to mars01

    Thanks for the info on process priority, however, for pouring polys it made no difference for me.

    I'm running a HP Z-book i7-7820HQ 16GB.

    The board I'm working on (approx 100x150mm) takes 8 seconds to pour two large polys, 4 secs to repour.

    Making the dxp process high priority didn't speed this up unfortunately.

     

    Who knows, maybe the CS code is pour_poly() then sleep(4000). That would not surprise me.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • mars01
    mars01 over 7 years ago in reply to voltsandjolts

    Yeah, just realized that on my newer notebook, the performance difference is not that big. For the pours I use a set of key shortcuts (P = Rebuild All and O = Set All to Unpoured)  and switch between those 2 states as needed. In a smallish projects (112 components and about 90 nets, 3 poly's) the change between poured and unpoured state is almost instant. But the polygons are not overlapped, they are 2 on top and one on bottom layer.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to mars01

    One useful tip of polygons do start to get slow (usually bring up the property dialog) is to split into two or three. I'm not certain but once the number of vertices increases (mainly due to components and tracks that are poured over rather than just size/area) the times increase exponentially (well non-linear) and splitting the polygon in two doesn't just half the time but can reduce back to pretty much zero. My understanding is that CS is mostly single threaded so perhaps difficult to boost performance by messing with process priorities. However I do remember going back many years to early hyperthreaded Pentiums that some FPGA software would run much faster once you turned off hyperthreading so always worth investigating ways of improving performance.