Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Polygons - automatic repour on error
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 13 replies
  • Subscribers 93 subscribers
  • Views 4386 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Polygons - automatic repour on error

GilchristT
GilchristT over 9 years ago

Folks

 

Am I missing something or is the "Automatic repour on polygon error" setting missing from the PCB Editor -> General settings screen?

 

If you make a change that requires a polygon repour the dialog gives you the option to change the setting but it's not there in version 1.4 unless I'm being particularly slow today?

  • Cancel

Top Replies

  • GilchristT
    GilchristT over 9 years ago in reply to e14softwareteam +1
    Sorry but I think you've missed my point. I've no problems repouring polygons, I just use the standard repour now and that resolves the issue. To give an example, say I've created a board design, placed…
Parents
  • e14softwareteam
    e14softwareteam over 9 years ago

    This is a previous response that may deal with this issue.  Let us know if this clarifies things:

     

    Currently CircuitStudio doesn't expose the pour order even though it is stored in the PCB file.

     

    The larger outer polygons need to be created last because newer polygons are poured last in the pouring order.

     

    To fix the board you will need to re-create the large outer polygon so that it pours after the others.

     

    Open the PCB panel and choose Polygons from the drop down list.

    Click <All Polygons> and then double click on the large polygon in the list of polygons names, e.g. TOP_GND

    Write down the settings (or take screen capture), e.g.

     

    Remove islands: 2 sq mm

    Arc approx: 0.013mm

    Necks: 0.127mm

    Name: TOP_1V2_C_1

    TopLayer

    Net: 1V2_C

    Pour over all same net objects

    remove dead copper

     

    Click the Outline Vertices tab at the top and click the Menu button > Export to CSV, name it, e.g. TOP_1V2_C_1

    Cancel out of the dialog and click on the document tab to take the focus back to the PCB document

    Press Delete to delete the polygon

     

    Press the Home > Polygon button, change the Name e.g. TOP_1V2_C_1 and draw a small simple polygon anywhere on the board

     

    Double click e.g. TOP_1V2_C_1 in the panel and ensure the correct Net is specified in teh Connect to Net setting.

    Click the Outline Vertices tab

    Menu > Import From CSV and double click on the CSV file e.g. TOP_1V2_C_1.csv

    Click back to the Graphical tab

    Ensure Is Poured is ticked and click OK

    Click Repour Now

     

    The Home > Polygon Pour > Repour All button should now repour the inner polygons before the new one you just created.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GilchristT
    GilchristT over 9 years ago in reply to e14softwareteam

    Sorry but I think you've missed my point.

     

    I've no problems repouring polygons, I just use the standard repour now and that resolves the issue.

     

    To give an example, say I've created a board design, placed some tracks and then a polygon pour for a ground plane. All good.

     

    I then decide to move a track slightly for some reason but this track now runs through part of the ground plane. CS will pop up a warning about the polygon needing repoured and asking me if I want to repour it now?

     

    I can do this and all is fine. However, in Altium Designer there's an option to enable this to happen automatically i.e. repour the polygon without a popup asking me if I want to do this.

     

    If is simply not available in CS as part of the deliberate crippling of the product to justify price points then that's fair enough but hte dialogue I mentioned above has a specific mention that this popup can be disabled in PCB Preferences so I assume that's either an error or the omission on the PCB preferences is an error.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • e14softwareteam
    e14softwareteam over 9 years ago in reply to GilchristT

    OK...I will pass this on to the developers for a reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GilchristT
    GilchristT over 9 years ago in reply to e14softwareteam

    Much appreciated, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • GilchristT
    GilchristT over 9 years ago in reply to e14softwareteam

    Much appreciated, thanks.