Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum v1.4 Hotfix Update Suggestions wanted here
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 16 replies
  • Subscribers 97 subscribers
  • Views 1866 views
  • Users 0 members are here
  • hotfix
  • bugs
  • patch
  • wants
  • features
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

v1.4 Hotfix Update Suggestions wanted here

jstrautman
jstrautman over 9 years ago

James Harriman mentioned in the discussion about not being able to create a board size based on 3D body as being a unintended bug and that the team is working on a "hotfix update" to version 1.4 to come soon.

 

I thought we  (the community) could start a list of items we would like to see updated as soon as possible.  These should be features that seem to hinder us as designers to designing a board quickly, efficiently, and correctly but easy enough to modify to be included in a short term software patch.

 

I'll kick it off by requesting that it be a priority to work on the Altium Vault Explorer search functionality.  There are many quirks with the Altium Vault Explorer, but the one that frustrates me the most is when you get many results, but can't view them because the results window is set up to automatically list a column for any parameter that was set up for any of the components.  It then requires me to go through and un-check many of them to get a usable view so I can expand the "Description" or "Comment" columns which is where I find what I'm looking for 99% of the time.  Sometimes there are over a hundred columns all checked and I have to get rid of 90 of them.  Can this search window just default to showing only the first few columns and let the user check which ones he/she wants to view.

 

Thanks for anyone else's input!

  • Cancel

Top Replies

  • a.teitlebaum
    a.teitlebaum over 9 years ago +2
    The rotation bug should definitely get fixed.
  • ninjaninja
    ninjaninja over 9 years ago +2
    just added the rotation bug again to this thread, as well as liking all the other people that stated this, Holy cow, that is a bad one!!! I have been using CS for a couple years and like it (seems like…
  • slowertech
    slowertech over 9 years ago in reply to ninjaninja +2
    This is the only thing I have run into that I felt really needed fixed in a hotfix. I wonder why it is taking so long and why they are not communicating.
Parents
  • jstrautman
    jstrautman over 9 years ago

    It also looks like in one of the early versions of CS there was an option to right click on a component in the Altium Vault and "Clone" the part which will allow you to easily use that part and modify it to keep in your own library.  This would be very handy to have again so I can have a custom version of a part if my design house has specific requirements for a part I use, or if there is a very similar part in the vault as a part that is not that I want to use.  I could then copy the vault part to my own library and do some small changes to make it the new part.

     

    As I understand it from other comments, the only way to do this now is to have a project open that you can drag the Vault component into.  Then you can have your library open with an empty footprint you created and copy the footprint of the Vault part and past it into your new footprint.  But I don't think the schematic editor will allow you to do this.  So for the moment I copy the footprint and start from scratch when making the component layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • jstrautman
    jstrautman over 9 years ago

    It also looks like in one of the early versions of CS there was an option to right click on a component in the Altium Vault and "Clone" the part which will allow you to easily use that part and modify it to keep in your own library.  This would be very handy to have again so I can have a custom version of a part if my design house has specific requirements for a part I use, or if there is a very similar part in the vault as a part that is not that I want to use.  I could then copy the vault part to my own library and do some small changes to make it the new part.

     

    As I understand it from other comments, the only way to do this now is to have a project open that you can drag the Vault component into.  Then you can have your library open with an empty footprint you created and copy the footprint of the Vault part and past it into your new footprint.  But I don't think the schematic editor will allow you to do this.  So for the moment I copy the footprint and start from scratch when making the component layout.