Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum v1.4 Hotfix Update Suggestions wanted here
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 16 replies
  • Subscribers 97 subscribers
  • Views 1864 views
  • Users 0 members are here
  • hotfix
  • bugs
  • patch
  • wants
  • features
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

v1.4 Hotfix Update Suggestions wanted here

jstrautman
jstrautman over 9 years ago

James Harriman mentioned in the discussion about not being able to create a board size based on 3D body as being a unintended bug and that the team is working on a "hotfix update" to version 1.4 to come soon.

 

I thought we  (the community) could start a list of items we would like to see updated as soon as possible.  These should be features that seem to hinder us as designers to designing a board quickly, efficiently, and correctly but easy enough to modify to be included in a short term software patch.

 

I'll kick it off by requesting that it be a priority to work on the Altium Vault Explorer search functionality.  There are many quirks with the Altium Vault Explorer, but the one that frustrates me the most is when you get many results, but can't view them because the results window is set up to automatically list a column for any parameter that was set up for any of the components.  It then requires me to go through and un-check many of them to get a usable view so I can expand the "Description" or "Comment" columns which is where I find what I'm looking for 99% of the time.  Sometimes there are over a hundred columns all checked and I have to get rid of 90 of them.  Can this search window just default to showing only the first few columns and let the user check which ones he/she wants to view.

 

Thanks for anyone else's input!

  • Cancel

Top Replies

  • a.teitlebaum
    a.teitlebaum over 9 years ago +2
    The rotation bug should definitely get fixed.
  • ninjaninja
    ninjaninja over 9 years ago +2
    just added the rotation bug again to this thread, as well as liking all the other people that stated this, Holy cow, that is a bad one!!! I have been using CS for a couple years and like it (seems like…
  • slowertech
    slowertech over 9 years ago in reply to ninjaninja +2
    This is the only thing I have run into that I felt really needed fixed in a hotfix. I wonder why it is taking so long and why they are not communicating.
Parents
  • harvie256
    harvie256 over 9 years ago

    I don't believe they should be adding anything beyond fixing what they broke from V1.3 in the hotfix.

     

    Any added "features" will delay this hotfix, and the hotfix will turn into another release.

     

    My current option in V1.4 is broken beyond being a usable release (due to component rotation bug.)  So I actually expect they would have fixed that and maybe the 3D board outline issue and released it by now.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • jstrautman
    jstrautman over 9 years ago in reply to harvie256

    You have a good point about quick release items needing to be focused on major problems.  Some of the problems I list are things I think have a chance of being a very minor bug that was introduced which would take just a couple lines of code to fix.

     

    Regarding your problems with v1.4...  James Harriman suggested in my question about the board shape from 3D body to install the old version 1.3 in parallel with my 1.4 installation and that worked well.  The two versions actually seem to work well together on my PC.  It will get me by until another update.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • GilchristT
    GilchristT over 9 years ago in reply to jstrautman

    +1 for component rotation bug - makes product practically unusable

     

    Hitting the [ESC] key in component properties in PCB view opens the component parameters dialogue rather than closing the dialogue.

     

    Repour Polygons on Error seems to be missing from the PCB Designer properties page despite being referenced in the dialogue that pops up when a polygon pour needs repoured due to a change

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • GilchristT
    GilchristT over 9 years ago in reply to jstrautman

    +1 for component rotation bug - makes product practically unusable

     

    Hitting the [ESC] key in component properties in PCB view opens the component parameters dialogue rather than closing the dialogue.

     

    Repour Polygons on Error seems to be missing from the PCB Designer properties page despite being referenced in the dialogue that pops up when a polygon pour needs repoured due to a change