Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CircuitStudio - Generate output files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 1743 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CircuitStudio - Generate output files

michael_n
michael_n over 9 years ago

How can I export 1 output file only? Every time when I select for example the BOM only and click on Generate, CS still export all kind of file like SCH, Gerber, NC Drill, PnP, Documentation....

Attachments:
image
  • Cancel

Top Replies

  • adamwebber
    adamwebber over 9 years ago +2
    The export feature for CS is absolutely horrible. Altium is soooooo much better. I find myself frustrated in most cases when I try to export files. So instead of using the check boxes on the export feature…
  • michael_n
    michael_n over 9 years ago in reply to adamwebber +1
    The more time I spend with CS, the more i miss AD
  • michael_n
    michael_n over 9 years ago +1
    I'd try to modify the Assembly Drawings-> Configure -> ok to add/remove layer "Mechanical 1" but can't add/remove "Mechanical 13" or "Mechanical 15" Just wonder how many programmer/tester are working on…
Parents
  • michael_n
    michael_n over 9 years ago

    I'd try to modify the Assembly Drawings-> Configure -> ok to add/remove layer "Mechanical 1" but can't add/remove "Mechanical 13" or "Mechanical 15"

    Just wonder how many programmer/tester are working on CS project. There're so many bugs!

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • michael_n
    michael_n over 9 years ago

    I'd try to modify the Assembly Drawings-> Configure -> ok to add/remove layer "Mechanical 1" but can't add/remove "Mechanical 13" or "Mechanical 15"

    Just wonder how many programmer/tester are working on CS project. There're so many bugs!