Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum "Find similar object" feature
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 16 replies
  • Subscribers 94 subscribers
  • Views 4697 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

"Find similar object" feature

jmarkwolf
jmarkwolf over 9 years ago

I’ve been using Altium, and Protel before
that, every day for about 20 years. I’m retiring shortly and have purchased
Circuit Studio for home use and consulting. I am pleased with my purchase decision.

 

One feature I’ve come to depend on in
Altium Designer is the “Find Similar Object”.

 

While upgrading some older Altium designs,
I needed to update schematic symbol parameters parts to reflect SMT footprints vs thru-hole
footprints. I found that I needed to manually select many parts across
multiple pages in order to make use of the schematic Inspector, which then allowed editing
the desired parameters. I’ll need to do this again to upgrade part numbers,
etc. Very tedious.

 

Please add the “Find Similar Object”
feature to Circuit Studio.

  • Cancel

Top Replies

  • voltsandjolts
    voltsandjolts over 7 years ago +4
    I apologise in advance for being a bit of a knob but.... I'm gonna keep bumping this thread because I think its important. I hope that someone from Altium will read it and take note.
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to voltsandjolts +3
    I apologise in advance for being a bit of a knob but.... I'm gonna keep bumping this thread because I think its important. I hope that someone from Altium will read it and take note.
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to voltsandjolts +3
    I apologise in advance for being a bit of a knob but.... I'm gonna keep bumping this thread because I think its important. I hope that someone from Altium will read it and take note.
Parents
  • e14softwareuk
    e14softwareuk over 9 years ago

    Many thanks for your suggestion, this is a very popular request that we have received several others. We have passed it on to Altium requesting them to consider this feature for a future release.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to e14softwareuk

    I'm digging up this old thread to prod the sleeping beast.

     

    This would be a very useful feature in schematic and pcb layout.

    If there were only one new feature added to CS in 2019 I would be happy if it was this.

     

    Any chance?

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to voltsandjolts

    If you have a board with several hundred vias with several different hole sizes, how do you select just the vias with 0.4 mm holes?

     

    How do you select only track segments that are 0.15mm wide?

     

    How do you select all resistors on a schematic that are 470R?

     

    AFAIK in CS the only way is to select them manually!

    The filters in CS are useful but only allow selection by object type and not by object parameters.

     

    The Select command has some useful methods but I can't see them all in the search results - maybe there is something in there?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to voltsandjolts

    It would be a manual job to select based on your criteria. Altium do have the Find Similar feature request logged as a suggestion (by several people) so we can only hope they are willing to add as it would be popular.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to e14softwareuk

    I have some hope that Find Similar Objects will be implemented in a future version of CS.

     

    I the meantime, CS Filters could be made much more useful with some small changes:

     

    (1) The "Text" Selection Filter (on the home ribbon) allows selection of individual designators but does not allow you to group select (click and drag over several components). I think this is a bug rather than an intentionally missing feature. Please allow click-drag group selection of designators with the Text filter.

     

    (2) Add a feature to the Filter tool which allows group selection of objects by some basic parameters.

    e.g. For PCB tracks "width". For vias "hole size".

    These basic parameters could be added as column(s) in the PCB Filter results (see below), thus allowing objects such as vias to be sorted by hole size and group selected (by multi-select in the Filter 'Highlighted Objects view').

    image

     

    One of the column headings (highlighted above in yellow) could perhaps be a drop-down list of sortable parameters for that object type.

     

    Note the above screenshot text highlighted in red "64 objects are passed the filter" should say "5 objects have passed the filter" because I have selected 5 in the Highlighted Objects list view. Small bug fix required.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • voltsandjolts
    voltsandjolts over 7 years ago in reply to e14softwareuk

    I have some hope that Find Similar Objects will be implemented in a future version of CS.

     

    I the meantime, CS Filters could be made much more useful with some small changes:

     

    (1) The "Text" Selection Filter (on the home ribbon) allows selection of individual designators but does not allow you to group select (click and drag over several components). I think this is a bug rather than an intentionally missing feature. Please allow click-drag group selection of designators with the Text filter.

     

    (2) Add a feature to the Filter tool which allows group selection of objects by some basic parameters.

    e.g. For PCB tracks "width". For vias "hole size".

    These basic parameters could be added as column(s) in the PCB Filter results (see below), thus allowing objects such as vias to be sorted by hole size and group selected (by multi-select in the Filter 'Highlighted Objects view').

    image

     

    One of the column headings (highlighted above in yellow) could perhaps be a drop-down list of sortable parameters for that object type.

     

    Note the above screenshot text highlighted in red "64 objects are passed the filter" should say "5 objects have passed the filter" because I have selected 5 in the Highlighted Objects list view. Small bug fix required.