Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Issues with Tending top and bottom
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 7 replies
  • Subscribers 89 subscribers
  • Views 1792 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Issues with Tending top and bottom

saravananeceait
saravananeceait over 8 years ago

Here I have attached an image please give me  the right solution for this !

Attachments:
image
image
  • Cancel

Top Replies

  • tarribred61
    tarribred61 over 8 years ago in reply to saravananeceait +1
    The basics of making a custom pad are to draw the shape(s) you want on the copper layer(s) and then copy the same shapes to the solder mask layer. Any shapes you draw on the solder mask layer will make…
Parents
  • saravananeceait
    saravananeceait over 8 years ago

    I need to create Custom pads ! in circuit studio software

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 8 years ago in reply to saravananeceait

    The basics of making a custom pad are to draw the shape(s) you want on the copper layer(s) and then copy the same shapes to the solder mask layer.  Any shapes you draw on the solder mask layer will make openings. It looks like you are not putting solder paste on the pads so you leave the solder paste layer alone.  If the pads are both the same on top and bottom then you only need to draw this as a surface mount component and place it on both sides of the board.  If you have vias connecting both sides, or want to electrically connect top and bottom pads,  then you can draw this as a single component and put the shapes on top and bottom copper and top and bottom solder mask and add the vias.  Or you could keep it as a single layer pad only and place one top and bottom then add stitching vias to connect at the PCB level. The link sent by Peter Barnard says something about how to assign a net name to the pads.

     

    I'd suggest making the pad in the PCB library and then placing on your board.  You can create a corresponding schematic library part that looks something like a simple test point or mounting hole and links to the PCB lib part with the custom footprint.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • tarribred61
    tarribred61 over 8 years ago in reply to saravananeceait

    The basics of making a custom pad are to draw the shape(s) you want on the copper layer(s) and then copy the same shapes to the solder mask layer.  Any shapes you draw on the solder mask layer will make openings. It looks like you are not putting solder paste on the pads so you leave the solder paste layer alone.  If the pads are both the same on top and bottom then you only need to draw this as a surface mount component and place it on both sides of the board.  If you have vias connecting both sides, or want to electrically connect top and bottom pads,  then you can draw this as a single component and put the shapes on top and bottom copper and top and bottom solder mask and add the vias.  Or you could keep it as a single layer pad only and place one top and bottom then add stitching vias to connect at the PCB level. The link sent by Peter Barnard says something about how to assign a net name to the pads.

     

    I'd suggest making the pad in the PCB library and then placing on your board.  You can create a corresponding schematic library part that looks something like a simple test point or mounting hole and links to the PCB lib part with the custom footprint.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • tarribred61
    tarribred61 over 8 years ago in reply to tarribred61

    I don't think CircuitStudio will let you convert selected lines into a polygon (Altium Designer does).  So instead you can place arcs and lines on a layer and then use them as guides to free hand draw the shape of the pad you want.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to tarribred61

    It is possible in CS to convert lines and arcs into polygons, use Polygon Pour > Define from Selected Objects menu command.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 8 years ago in reply to e14softwareuk

    Hi Peter,

     

    I think you can do that in the PCB level but not at the PCB library level.  You might be able to do it on the PCB level and then cut and paste a shape into the PCB library though.