Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Capacitors connected GND to GND
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 7 replies
  • Subscribers 93 subscribers
  • Views 4351 views
  • Users 0 members are here
  • rf adc
  • adc to fmc
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Capacitors connected GND to GND

saravananeceait
saravananeceait over 8 years ago

Why capcitors connected Ground to ground ? what is the need? and what is the value of these capacitors?

Attachments:
image
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +5
    Hi, It's just to get rid of any static charges, when the board is inserted into the chassis. This is because the edge is going to be the first bit that touches the chassis, and the capacitors have physically…
  • adamwebber
    adamwebber over 8 years ago +2
    Just a wild guess but maybe there are two isolated grounds on the PCB. Also, this forum is not necessarily for circuit-technical questions. It's pretty much for CircuitStudio-related questions.
  • jw0752
    jw0752 over 8 years ago +1
    Your question came through on main Forum Stream too so there is a pretty good chance that someone smarter than me will respond. What makes you think that both sides of the capacitor are connected to ground…
Parents
  • rachaelp
    rachaelp over 8 years ago

    So judging by their location right next to connectors and that there is one each side of the board and they connect to an exposed copper area running around the perimeter of the board, presumably for an electrical connection to a chassis that fastens around the board, I would say they are likely AC coupling between the chassis ground and the main ground of the circuit so they are connected as far as AC signals are concerned but they remain isolated as far as DC voltages are concerned.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • rachaelp
    rachaelp over 8 years ago

    So judging by their location right next to connectors and that there is one each side of the board and they connect to an exposed copper area running around the perimeter of the board, presumably for an electrical connection to a chassis that fastens around the board, I would say they are likely AC coupling between the chassis ground and the main ground of the circuit so they are connected as far as AC signals are concerned but they remain isolated as far as DC voltages are concerned.

     

    Best Regards,

     

    Rachael