Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Arrange components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 5 replies
  • Subscribers 91 subscribers
  • Views 1362 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Arrange components

pat180269
pat180269 over 8 years ago

In a multi-sheet design its handy to be able to select all the pcb components associated with a sheet and move them to an area of the board ready for placement and routing.

I can select all the PCB components by clicking SELECT->CROSS SELECT MODE in the sheet schematic.

But how do I move/arrange the selected components in a given area of the board ?

  • Cancel
Parents
  • e14softwareuk
    e14softwareuk over 8 years ago

    Also worth knowing that components on the PCB are automatically added to a component class based on schematic sheet name (e.g. Sheet1, Sheet2). Bring up the PCB pane using View > PCB > Components and then click on a component class. This will select all the chosen components which can then be moved as a group. Use the View > Clear option to end filtering.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    e14softwareuk over 8 years ago

    Also worth knowing that components on the PCB are automatically added to a component class based on schematic sheet name (e.g. Sheet1, Sheet2). Bring up the PCB pane using View > PCB > Components and then click on a component class. This will select all the chosen components which can then be moved as a group. Use the View > Clear option to end filtering.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • pat180269
    pat180269 over 8 years ago in reply to e14softwareuk

    Thanks Peter/Rachael. Once selected is there a way of moving and clustering the components together into a given area of the board? The Arrange ( Move Align ) has lots of functions but I don't see this. I suppose I'm looking for the equivalent to the Protel function "Arrange components within defined area". The area was defined by drawing a box.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to pat180269

    I don't think there is an automated way to cluster components together into a defined area.