Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Did you guys even beta test this?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 15 replies
  • Subscribers 90 subscribers
  • Views 1765 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Did you guys even beta test this?

naca6409
naca6409 over 8 years ago

I've been trying to get used to Circuit Studio after being trained on Altium, and I'm going to say straight off: This software is *extremely* disappointing.  No "Find Similar"?  Sure, remove the flex circuit functionality, but keep the basic productivity features!

 

Anyways, my reason for creating an account and posting was this train-wreck:

image

 

I'm using the software on a Surface Book 2.  Fresh install, both OS and CircuitStudio.  I haven't screwed with any display settings or anything.  It's as stock as things can get.


However, for some reason, the "Cartesian Grid Editor" aka "Snap Grid" dialog in the PCBLib editor is not rendering correctly, making it impossible for me to adjust the values.

  • Cancel
Parents
  • csiemer
    csiemer over 8 years ago

    What resolution are you currently running at? 

     

    Minimum resolution for CircuitStudio is currently 1280x1024 at 100% scaling

     

    So, if you are at 1024 or around there, and scaling is set higher than 100% within Windows, some dialogs can get a chop effect like you are seeing here.  If you are at or below 1024, and also at a higher scaling it could end up looking like your screenshot.

     

    If your maximum vertical resolution cannot reach 1024, you will have to run at 100% scaling for CircuitStudio, and some dialogs might still be difficult to see.  But in these cases, please let us know the resolution and scaling you are running at and if it is a dialog we can improve, we can submit a ticket for review.

     

    This table is pretty handy for mapping scaling to resolution for CircuitStudio, I hope it helps, but keep in mind that even at Maximum scaling for a resolution, on widescreen ratios I have still seen some minor dialog chopping so although it might say 250%, if you see a dialog chopped, try dropping to 200% and see if it improves.

    Scaling is changed within Windows 10 by accessing your Display Settings in the Scale and Layout section.

    Monitor Vertical Resolution (pixels)Maximum DPI Scaling Supported
    1024 to 1200100%
    1600125%
    1800200%
    2K and above250%
    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • naca6409
    naca6409 over 8 years ago in reply to csiemer

    As I mentioned before, this is stock Windows 10 on a Surface Book 2.  I haven't changed any settings, but my current display settings are within the ranges your table specifies.  I also tried a second display (2560x1440 @ 100% scale) with no change.




    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • csiemer
    csiemer over 8 years ago in reply to naca6409

    Hmm, should definitely look close to how I see mine, your settings are not too different than how I run.

     

    If you are not comfortable changing the registry, but are comfortable having a look, can you please go to the Registry key Peter referenced above and take a screenshot of the values?

    HKEY_CURRENT_USER\Software\Altium\CircuitStudio {guid}\DesignExplorer\Forms\TGridEditorForm

     

    As a reference, here is how mine look for this particular form.

    image

     

    I am curious if your values are somehow different, maybe an issue during install or something.  At minimum we can get a ticket submitted to make this dialog resizable, but my troubleshooting brain is curious as to the cause of this so hopefully we can get to the root of it image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • naca6409
    naca6409 over 8 years ago in reply to csiemer

    Good idea.  I tried adjusting the height parameter to match yours and the behavior of the dialog was the same when I next invoked it. image

     

    imageimage

     

    Previously, the value was set to 240.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • csiemer
    csiemer over 8 years ago in reply to naca6409

    Ok, one more thing to check settings wise.

     

    For the shortcut you use to open CircuitStudio, access the properties of this shortcut and then go to the Compatibility tab.  There is a section here for High DPI scaling.  Please take a screenshot of this so I can see how it is set.

    Here are the regular settings I use for reference

    image

    I tried various options here to reproduce what you are seeing, but could not do it.  However, in changing these settings the dialog is modified.  So, it might be worth checking a few of the settings here to see if they either correct the issue, or at least kick that dialog into a readable/usable size.  To see changes with this, you will need to close and re-launch CircuitStudio from the updated shortcut properties.

     

    Also, just to be sure, check to see that you have all critical Windows updates installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • naca6409
    naca6409 over 8 years ago in reply to csiemer

    Here were my settings.  I tried mirroring yours and did not get any change in behavior.

    image

    My updates are current.  image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to naca6409

    This grid dialog is used by the the PCB and PCBLIB editors, do you get the same dialog issue from both editors?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to naca6409

    This grid dialog is used by the the PCB and PCBLIB editors, do you get the same dialog issue from both editors?