Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Differential pairs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 9 replies
  • Subscribers 90 subscribers
  • Views 2316 views
  • Users 0 members are here
  • frontpage
  • differential pairs
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Differential pairs

Sparkylabs
Sparkylabs over 8 years ago

Firstly I'd like to point out that the CS video on differential pairs is just one level above non existent.

 

So as per the video I create "a pair" but I have 2 differential pair nets in my schematic, if I just click on one of the diff. pair symbols i see that it has a generic name like diffpair. Do I correctly assume (yes we have to use assumption instead of actual documentation!) that for multiple differential pairs this name needs to be specific to the pair or i will have 4 traces that belong to the same "pair" set?

  • Cancel
Parents
  • Sparkylabs
    Sparkylabs over 8 years ago

    OK so I got as far as trying to route the PCB. So diff. pairs between multiple points is a waste of time, once a pair between 2 locations has been done it's impossible to run a "pair" to the 3rd location. I ended up doing that by hand while noting that the connections must be point to point so both pins at both ends on the right side. I mean frankly the use of routing diff. pairs is just about usable.

     

    When will altium be "bothered" to both write a comprehensive manual and if they are going to waste their time making videos perhaps they can make complete videos, I am yet to see one that fully describes a function.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to Sparkylabs

    Just tested with very simple design and you can have more than two connections. It's not intended to be a sensible design but it worked by routing each pair segment one at a time, i.e. complete one pair and then start routing the next pair segment.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to Sparkylabs

    Just tested with very simple design and you can have more than two connections. It's not intended to be a sensible design but it worked by routing each pair segment one at a time, i.e. complete one pair and then start routing the next pair segment.