Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum CircuitStudio gets extremly slow with polygon
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 7 replies
  • Subscribers 90 subscribers
  • Views 1560 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

CircuitStudio gets extremly slow with polygon

tomaszciesla
tomaszciesla over 8 years ago

Hi all,

We've faced a problem while working on bigger PCB and polygon pour:

- PCB has about 2k elements

- 1 polygon on bottom layer connected to GND, solid pour.

When you double click on polygon to edit it it takes 15 minutes on laptop to get the polygon properties window (Dell 7480/i7). After moving to workstation (new Dell XPS i7) it takes 3 minutes!! Task manager shows full load of one core / process

Polygon rebuild takes same time. It's funny because it seems that rebuilding is fast, but accessing polugon's properties takes ages.

  • Cancel
Parents
  • e14softwareuk
    e14softwareuk over 8 years ago

    This is an issue that we have very occasionally encountered before so we do have a couple of suggestions. Please give these a try and let us know which works for you.

     

    1) Try adjusting the polygon properties, unset the two options shown.

    image

     

    2) Use a hatched polygon with properties set so that it is actually filled, set the track width and grid to the same value (e.g. 1mil).

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tomaszciesla
    tomaszciesla over 8 years ago in reply to e14softwareuk

    Hi, thanks for quick reply, but it didn't help.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • tomaszciesla
    tomaszciesla over 8 years ago in reply to e14softwareuk

    Hi, thanks for quick reply, but it didn't help.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to tomaszciesla

    If you have tried both suggestions then are you able to share the PCB with me, no need to post on forums just directly email?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tomaszciesla
    tomaszciesla over 8 years ago in reply to e14softwareuk

    we can share PCB on email, please pw me or post your email

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to tomaszciesla

    Thanks for sharing. Best solution I can find up to now is delete the polygon and replace with a number of smaller ones (I tried 8 horizontal strips). You can safely overlap to create one large seamless copper area because the polygons are all the same net and set to cover same net objects. This seems to improve things from several minutes to 10 seconds or better.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to e14softwareuk

    Another hint that seems to speed up operations considerably to add to the above. If using solid fill try setting the Arc Approximation to a larger value, I tried 0.1mm and this reduced the time from around 10 seconds to under 2 seconds. If using hatched then try using Surround Pads With Octagons rather then Arcs.