Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Net length is wrong (vias isn't taken into account)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 14 replies
  • Subscribers 91 subscribers
  • Views 2912 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Net length is wrong (vias isn't taken into account)

a.stepanov
a.stepanov over 8 years ago

Hi!

 

Routed length calculation is wrong (vias height does not taken into account).
CS version is 1.4.1 build 99.
When it will be fixed ?

 

Thanks!

Attachments:
image
  • Cancel
Parents
  • voltsandjolts
    voltsandjolts over 8 years ago

    To match a diff pair you should be using the same number of vias in _P and _N and thus via length is of no consequence.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • a.stepanov
    a.stepanov over 8 years ago in reply to voltsandjolts

    Thanks for the reply.

     

    Sure! This is just an example.

     

    Real problem is observed when I need to match differential pair length to data bus as well as route all signals inside data bus.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 8 years ago in reply to a.stepanov

    In that case, you will need to manually add up via lengths which is non-trivial for more complex stack-ups. Or pony up several thousand dollars and upgrade to Designer.

     

    Altium decided to leave the via length feature out of CS, which seems fair enough to me for its target market and cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • a.stepanov
    a.stepanov over 8 years ago in reply to voltsandjolts

    Are you seriously ?

    If so, I'm can't agree with you.

    When we are talking about trace matching tool, yes, this is a "feature" available in more expensive package.

    But when net length is showed without simple distance between layers this is just a "bug".

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • voltsandjolts
    voltsandjolts over 8 years ago in reply to a.stepanov

    Yes, absolutely serious.

    The target market for CS is where via length is unimportant or is at least trivial to manually calculate.

    How many hundred MHz is your design operating at and who are you using to manufacture your controlled impedance boards? Doesn't sound like entry level PCB design to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • a.stepanov
    a.stepanov over 8 years ago in reply to voltsandjolts

    Good product should have balance of available features.

    CS has net classes, diff pair routing, multilayer stack-up, but on other hand simple via length does not automatically calculated.

    More expensive products like Altium have much more other usefull features.

    Via length is not feature nowadays. It is one of  "must have" options today.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • a.stepanov
    a.stepanov over 8 years ago in reply to voltsandjolts

    Good product should have balance of available features.

    CS has net classes, diff pair routing, multilayer stack-up, but on other hand simple via length does not automatically calculated.

    More expensive products like Altium have much more other usefull features.

    Via length is not feature nowadays. It is one of  "must have" options today.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • voltsandjolts
    voltsandjolts over 8 years ago in reply to a.stepanov

    A "must have" for high frequency controlled impedance designs, yes.

    But you're not actually using controlled impedance boards, are you? In which case your via lengths don't mean diddly-squat.