Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum What is the rubber stamp and can it be used to copy settings between objects
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 90 subscribers
  • Views 1409 views
  • Users 0 members are here
  • unsolved mystery
  • pcb editor
  • rubber stamp
  • circuitstudio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What is the rubber stamp and can it be used to copy settings between objects

jaza_tom
jaza_tom over 7 years ago

I am trying to set multiple pads solder mask expansion value to be 10 mil

 

Unfortunately when viewing multiple selected pads using PCB Inspector tool, no entry can be found for solder mask expansion value:

image

 

So, I switched my focus to trying to find a command that can be used to copy an objects' parameters and paste as parameters into a second object.

 

I thought that perhaps the Rubber Stamp tool could do that (access by typing "Rubber" into the command search bar in upper right of CircuitStudio window):

image

 

Unfortunately, as far as I can tell, this command does not actually do anything.  So what is it supposed to do?

  • Cancel

Top Replies

  • frog
    frog over 7 years ago +1
    Interestingly, I don't have a rubber stamp command at all (CS 1.5.2 build 30)
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to frog +1
    Confirmed - it doesn't existing in 1.5.2. A little more digging shows that rubber stamp does exist - if you have something already selected. It is basically copy & paste. There is no way to manually edit…
  • tarribred61
    tarribred61 over 7 years ago in reply to jaza_tom +1
    It seems to refer to an older command in AD that was deprecated in AD18. It was discussed in this link I got on a web search that ended up downloading a PDF doc. I used Google to find this string "altium…
Parents
  • frog
    frog over 7 years ago

    Interestingly, I don't have a rubber stamp command at all (CS 1.5.2 build 30)

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • frog
    frog over 7 years ago

    Interestingly, I don't have a rubber stamp command at all (CS 1.5.2 build 30)

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • e14softwareuk
    e14softwareuk over 7 years ago in reply to frog

    Confirmed - it doesn't existing in 1.5.2.

    A little more digging shows that rubber stamp does exist - if you have something already selected. It is basically copy & paste.

     

    There is no way to manually edit the solder mask expansion of multiple pins in one go. However the automatic mask expansion is part of the design rules so depending on what you are looking to achieve you may be able to add a new expansion rule and tie in with a component, footprint or pad class.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • jaza_tom
    jaza_tom over 7 years ago in reply to e14softwareuk

    Here is the version that I have installed:

     

    image

     

    Seems like I am also running 1.5.2

     

    I guess this command somehow either was introduced into a beta release or else is left over somehow after I downloaded updates.

     

    Whatever.... lets just file this in the "unsolved mystery" category.  Adding tag now.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    tarribred61 over 7 years ago in reply to jaza_tom

    It seems to refer to an older command in AD that was deprecated in AD18.

     

    It was discussed in this link I got on a web search that ended up downloading a PDF doc.  I used Google to find this string "altium rubber stamp PCB"

    http://techdocs.altium.com/printpdf/210230

     

    And so you don't have to follow the link here is a screen shot.