Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Still having issues with Printer Driver for Output Generation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 89 subscribers
  • Views 791 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Still having issues with Printer Driver for Output Generation

adamwebber
adamwebber over 7 years ago

A Couple of years ago I got an Epson ET-3750 Printer.  After I installed the driver, none of my output generation PDF files came out correctly.  They are all shrunk to about 60%.  I cannot find a workaround for them.  It used to be really nice when I could click on a component and it would display all of the data relating to that part.  I can still click on the parts (at 100%) but it's a guessing game as to where the location will be since it displays the sheets on a smaller scale (at 60%).  I've tried updating the printer driver, uninstalling it, changing it, but to no avail.  It's like it's stuck in this mode now.  Included is an example of a development board I designed last year.

 

Is there any way that I can fix this problem?  It's quite annoying and doesn't help when I create a project for a client.

Attachments:
image
  • Cancel
Parents
  • e14softwareuk
    e14softwareuk over 7 years ago

    Hi James. Does it make a difference if you install a completely different printer driver (e.g. PDF generator printer), set as the default and then try printing to this printer?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • adamwebber
    adamwebber over 7 years ago in reply to e14softwareuk

    What is interesting is that if I go to the 'Outputs' tab and select 'Print Preview' under the 'Print' option, the sizing is reduced.  But if I select 'Page Setup' and click 'Preview', the scaling is correct.  But this only works for a single sheet at a time and it doesn't embed the properties of the components into the PDF file.

     

    I will try clearing the settings but I'm going to make a copy first.  It takes a while to get everything set up just the way I like it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • adamwebber
    adamwebber over 7 years ago in reply to e14softwareuk

    What is interesting is that if I go to the 'Outputs' tab and select 'Print Preview' under the 'Print' option, the sizing is reduced.  But if I select 'Page Setup' and click 'Preview', the scaling is correct.  But this only works for a single sheet at a time and it doesn't embed the properties of the components into the PDF file.

     

    I will try clearing the settings but I'm going to make a copy first.  It takes a while to get everything set up just the way I like it.