AMD
  • Products & Partners
  • Manufacturers
  • AMD
  • More
  • Cancel
AMD
Forum FMC Connectors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join AMD to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 52 subscribers
  • Views 2102 views
  • Users 0 members are here
  • zc702
  • fmc
  • fmc_lpc
  • vita_57.1
  • lpc
Related

FMC Connectors

14rhb
14rhb over 7 years ago

I was trying to make a breakout board for the Xilinx ZC702 and specifically to be able to utilise the FMC pinouts. I believe the board uses the Samtec ASP-134603-01ASP-134603-01 Low Pin Count (LPC) connector but looking at their website I am uncertain what the mating part is. I've narrowed it down to ASP-134604-04 or ASP-134606-04 (the leaded option rather than lead-free) - the difference is described as:

VITA Standards specify configurations for the SEARAYTm High-Speed Array VITA 57.1 FPGA Mezzanine Card (FMC) connector in 8.5 mm and 10 mm stack heights.

But I cannot work out what that actually means and which I should buy. Any advice would be appreciated.

image

Rod

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago +3
    When I needed to access those pins (on a different Xilinx board) I used a Cypress dev board adaptor. A bit wacky but it worked OK and was cheap. CYUSB3ACC-005 RS and Farnell have no stock but Mouser have…
  • 14rhb
    14rhb over 7 years ago +2
    As an update: I had also contacted Samtec.com and they have explained that the stack height is the distance between the two boards when the connectors are mated together...which is so obvious now. I could…
  • 14rhb
    14rhb over 7 years ago in reply to michaelkellett +1
    Thank you Michael. That board also mitigates against my next worry - the connectors are pre-loaded with solder for SMT reflow. I haven't got such equipment and was hoping to flood solder along & underneath…
Parents
  • 14rhb
    14rhb over 7 years ago

    As an update:

     

    I had also contacted Samtec.com and they have explained that the stack height is the distance between the two boards when the connectors are mated together...which is so obvious now. I could opt for either but the closer 8.5mm could mean my board fouls on ZC702 components and therefore the 10mm clearance is recommended, which is ASP-134604-04 (leaded) or ASP-134604-02 (lead free).

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    And here is the new connector, which fits my ZC702 FMC LPC connector....time to crack on with the Logic Analyser.

    image

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    And here is the new connector, which fits my ZC702 FMC LPC connector....time to crack on with the Logic Analyser.

    image

    Rod