Analog Devices
  • Products & Partners
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum PROBLEM whith MAX17632C
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 46 subscribers
  • Views 2071 views
  • Users 0 members are here
Related

PROBLEM whith MAX17632C

Fabrizio70
Fabrizio70 over 2 years ago

v   image

Hi , I have a problem whith  max17632c i use it for dc/dc 24v/5v  .if i put  i small load ( 100mW) the output voltage is 4,0V  , while i put a load of  2W  tthe output voltage go to 2,5V.

then i desolder  the condensator  C1 (2,2 uF 10V ceramic used for bypass ldo pin 2) and i have 5v output  whit load of 2W (the condensator  not  have problem) , Where is the prblem?

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 2 years ago +1
    Since it is a switching regulator, we need to see the PCB. I always suspect layout issues first with switchers. It would also be nice to see the entire schematic. Like with code, snippets rarely contain…
  • Fabrizio70
    Fabrizio70 over 2 years ago in reply to dougw +1 verified
    The output voltage whiout load and c1 installade is 5,09 V , while whit load of 2W and c1 installated is 2,35 v and the voltage on the C1 is 5,06 if i dessolder c1 the output voltage is right 5.06 whit…
Parents
  • dougw
    0 dougw over 2 years ago

    What is the voltage at VCC when the cap is installed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Fabrizio70
    +1 Fabrizio70 over 2 years ago in reply to dougw

    The output voltage whiout load  and c1 installade is 5,09 V , while  whit load of 2W and c1 installated is 2,35 v and the voltage on the C1 is 5,06  if  i dessolder c1  the output voltage is right 5.06 whit load of 2W

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • baldengineer
    0 baldengineer over 2 years ago in reply to Fabrizio70

    Are you looking at the output with an oscilloscope or a DMM?

    Remember, DMMs do not show you the full picture with a switch-mode regulator,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Fabrizio70
    0 Fabrizio70 over 2 years ago in reply to baldengineer

    whith multimeter, if i use oscilloscope i measure a ripple of 1v on pin 2 (VCC) WHITOUT C1 while whit  c1x the riplle is a some mV but the output (MEASURE ON c19)  whitl load is 2,35V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Fabrizio70
    0 Fabrizio70 over 2 years ago in reply to baldengineer

    whith multimeter, if i use oscilloscope i measure a ripple of 1v on pin 2 (VCC) WHITOUT C1 while whit  c1x the riplle is a some mV but the output (MEASURE ON c19)  whitl load is 2,35V