BitScope
  • Products & Partners
  • Manufacturers
  • BitScope
  • More
  • Cancel
BitScope
Forum New PoE Bitscope product for PoE and Raspberry Pi 3B+ mentioned in blog post
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BitScope to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 35 subscribers
  • Views 866 views
  • Users 0 members are here
  • poe hat
  • bitscope
  • raspberry pi 3b+
  • poe
Related

New PoE Bitscope product for PoE and Raspberry Pi 3B+ mentioned in blog post

accipiter
accipiter over 8 years ago

The following blog post mentioned a new BitScpoe product that was described as likely to be available at about the same time as the Raspberry Pi PoE Hat (now available...):

 

https://www.element14.com/community/community/raspberry-pi/blog/2018/03/15/bitscope-reviews-raspberry-pi-3-model-b

 

There was very little detail in the post apart from one CAD diagram with Bi3B+ in situ.

 

Is there any more detail?  I was hoping that it could accept a PoE directly without an external splitter and utilise Bitscope board's more robust power management and breakout several more 5V feeds in addition to the Pi3B+'s USB ports which the new Raspi Foundation new PoE board wont do as far as I can see.

 

Thanks image

  • Sign in to reply
  • Cancel
Parents
  • bitscope
    0 bitscope over 8 years ago

    It's coming real soon now. It accepts PoE via the B+ LAN connector (like the PoE HAT). It has the same robust BitScope Blade onboard power regulation (supports 12V-48V), mounts in a similar way to existing Blades, can be used stand-alone or in racks, provides a breakout for a 5V feed for external circuits and supports third party HATs. It actually does quite a bit more than this, but we'll leave the details for the launch (hopefully in a month or so).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bitscope
    0 bitscope over 8 years ago

    It's coming real soon now. It accepts PoE via the B+ LAN connector (like the PoE HAT). It has the same robust BitScope Blade onboard power regulation (supports 12V-48V), mounts in a similar way to existing Blades, can be used stand-alone or in racks, provides a breakout for a 5V feed for external circuits and supports third party HATs. It actually does quite a bit more than this, but we'll leave the details for the launch (hopefully in a month or so).