BitScope
  • Products & Partners
  • Manufacturers
  • BitScope
  • More
  • Cancel
BitScope
Forum Waveform generator limitations
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BitScope to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 37 subscribers
  • Views 2267 views
  • Users 0 members are here
  • waveform limits probe compensation
Related

Waveform generator limitations

AussieSusan
AussieSusan over 5 years ago

I have linked the analog output to the analog input as part of testing and getting to know the Bitscope Micro. When generating lower-end frequencies (sine wave in this case) the received waveform is quite clean.

However when setting the frequency to the top of the range, it looks like some harmonics are being introduced. Also when using square waves, there is considerable overshoot on the transitions.

Therefore, is there some practical limit to the frequency the waveform generator can be used to get 'clean' waveforms?

Alternatively, am I just seeing a poorly compensated 'probe' (especially with the square wave)? If that is gthe case, is there a way to adjust the probe compensation (as there is typically with a 'normal' DSO probe)?

Susan

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 5 years ago +3 verified
    It appears the Bitscope Micro runs the waveform generator DAC at a sample rate of 1 MHz (Not exactly sure). So without any additional filtering on the output I wouldn't expect to see "clean" sine waves…
  • Jan Cumps
    Jan Cumps over 5 years ago +2
    Do you have to terminate the waveform output with 50 Ohm load?
  • AussieSusan
    AussieSusan over 5 years ago +2
    (Sorry - distracted by life!) Thanks for the responses. @JanCumps - no I didn't specifically terminate the waveform output but, as I said in the first posting, I looped it back to the analog input - if…
  • Jan Cumps
    0 Jan Cumps over 5 years ago

    Do you have to terminate the waveform output with 50 Ohm load?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 5 years ago

    It appears the Bitscope Micro runs the waveform generator DAC at a sample rate of 1 MHz (Not exactly sure). So without any additional filtering on the output I wouldn't expect to see "clean" sine waves really past 10 kHz.

     

    Depending on how detailed of an answer you are looking for, you can take a look at: https://www.analog.com/media/en/training-seminars/design-handbooks/Technical-Tutorial-DDS/Section2.pdf to define an exact distortion specification.

     

    If you can add an RC reconstruction filter to reject some of the sample images you will see the sine distortion improve.

     

    Probe Compensation: I have never used a Bitscope scope so I'm not really sure, but probe compensation would only apply to a 10x probe, I'm not sure if that is what is included with the scope.

     

    All the best!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • AussieSusan
    0 AussieSusan over 5 years ago

    (Sorry - distracted by life!)

    Thanks for the responses.

    @JanCumps - no I didn't specifically terminate the waveform output but, as I said in the first posting, I looped it back to the analog input - if that has a 50Ohm termination then 'yes' otherwise "I don't know'.

    @ScottStobbe - thanks for the information. As for the probe compensation, I guess I've been dealing with analog and digital scopes for nearly 50 years now and old habits die hard.

    Susan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to AussieSusan

    I expect that the signal integrity will be closer to expectation if it's properly terminated with 50 Ohm just before the input.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer