Bulgin
  • Products
  • Manufacturers
  • Bulgin
  • More
  • Cancel
Bulgin
Blog Whats the difference between a capacitive switch and a piezo switch?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Bulgin to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bulgin
  • Date Created: 25 Nov 2019 11:57 AM Date Created
  • Views 1045 views
  • Likes 0 likes
  • Comments 0 comments
  • switches
  • piezo
  • capacitive
Related
Recommended

Whats the difference between a capacitive switch and a piezo switch?

bulgin
bulgin
25 Nov 2019

If you have ever had to research switches or even select a switch for a piece of electronic equipment, the number of switch technologies available on the market today might be a little overwhelming. This blog post will focus on two switches that look very similar but function according to completely different electronic principles. The question is: just what is the difference between a piezo switch and a capacitive touch switch?

First, let us examine some of the aspects that the two have in common.

Both types of switches are usually comprised of flat, metallic discs, sometimes surrounded by an illuminated ring that lights up when the switch is activated.

Typically they are installed flush with the control panel, and with no moving parts they are often highly wear-resistant, dustproof, waterproof and suitable for repetitive operation. The durability of these switches means they can withstand millions of actuations and require little to no maintenance.

Piezo switches

A piezo is a small disc comprised of two layers; an inner ceramic layer and an outer layer usually made from a metallic substance. It reacts to the force of being touched and generates an electric charge, which effectively sends a signal that the button has been pushed.

A piezo switch relies on mechanical displacement or bending of piezo ceramic – also known as the piezoelectric effect. The word piezo is derived from the Greek piezein, which means to squeeze or press. While there are no mechanical moving parts within the switch, it does require sufficient pressure to be applied in order to deflect the ceramic layer within.

Capacitive switches

On the other hand, a capacitive switch, also known as a capacitance switch, requires just one electrode, which can be placed behind a non-conductive panel. The switch uses body capacitance, making use of the electrical charge naturally carried by the human body. The difference between the device itself and the fingertip is sensed, thereby triggering the switch.

How to choose between the two:

A piezo switch senses touch force or relies on a small force, while capacitive switches require a charge or electrode, typically generated from human touch. So for devices that are meant to react only to human touch, then the capacitive touch switch is ideal for this purpose.

Capacitive switches are used in a wide selection of applications, from medical and laboratory equipment and food processing machinery to consumer applications such as appliances, vending machines and lift controls.

Price wise, capacitive switches are typically cheaper than piezo switches from a raw materials perspective.

A user wearing thick gloves cannot operate a capacitive switch. They do however work with thin surgical gloves or specially designed conductive fibre gloves that will allow a charge to be passed from the hand to the switch. This is where the piezo switch truly comes into its own – these switches will function regardless of the type of glove the user is wearing as the switch depends on pressure to operate, not human touch.

Bulgin’s range of piezo switches are vandal-resistant, waterproof and dust proof with an ingress protection rating of IP68 and IP69K, and the company’s range of highly durable capacitive touch switches will also soon be released.

For more information about Bulgin's piezo switches please visit: www.bulgin.com